<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic OM5577/PN7120S compatability with Raspberry Pi 3 B+ in NFC</title>
    <link>https://community.nxp.com/t5/NFC/OM5577-PN7120S-compatability-with-Raspberry-Pi-3-B/m-p/903950#M5427</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have tried using the demo images provided to run the PN7120 on Raspberry Pi 3 B+; however, all of them have the rainbow screen, indicating a failed boot. Additionally, I tried installing the software stack on a new image of Raspbian, but it is not communicating via i2c. Any demo or tutorial that I try to follow fails with a communication error via i2c. If Pn7120 is compatible with raspberry pi 3 b+, is there a demo image that has already been configured?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 21 Apr 2019 15:11:24 GMT</pubDate>
    <dc:creator>jdavidson2019</dc:creator>
    <dc:date>2019-04-21T15:11:24Z</dc:date>
    <item>
      <title>OM5577/PN7120S compatability with Raspberry Pi 3 B+</title>
      <link>https://community.nxp.com/t5/NFC/OM5577-PN7120S-compatability-with-Raspberry-Pi-3-B/m-p/903950#M5427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have tried using the demo images provided to run the PN7120 on Raspberry Pi 3 B+; however, all of them have the rainbow screen, indicating a failed boot. Additionally, I tried installing the software stack on a new image of Raspbian, but it is not communicating via i2c. Any demo or tutorial that I try to follow fails with a communication error via i2c. If Pn7120 is compatible with raspberry pi 3 b+, is there a demo image that has already been configured?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 21 Apr 2019 15:11:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM5577-PN7120S-compatability-with-Raspberry-Pi-3-B/m-p/903950#M5427</guid>
      <dc:creator>jdavidson2019</dc:creator>
      <dc:date>2019-04-21T15:11:24Z</dc:date>
    </item>
    <item>
      <title>Re: OM5577/PN7120S compatability with Raspberry Pi 3 B+</title>
      <link>https://community.nxp.com/t5/NFC/OM5577-PN7120S-compatability-with-Raspberry-Pi-3-B/m-p/903951#M5428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a Raspberry Pi 3 B ver 1.2 on hand and it works well with OM5577, but I am not sure if B+ is also the same, let me&amp;nbsp; check it later.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will let you know when I have any more info.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your patience!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Apr 2019 09:00:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM5577-PN7120S-compatability-with-Raspberry-Pi-3-B/m-p/903951#M5428</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-04-23T09:00:31Z</dc:date>
    </item>
    <item>
      <title>Re: OM5577/PN7120S compatability with Raspberry Pi 3 B+</title>
      <link>https://community.nxp.com/t5/NFC/OM5577-PN7120S-compatability-with-Raspberry-Pi-3-B/m-p/903952#M5429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have got the Raspberry Pi 3B+ board and met the same issue, but when I burn the latest image from &lt;A href="https://downloads.raspberrypi.org/raspbian_full_latest" title="https://downloads.raspberrypi.org/raspbian_full_latest"&gt;https://downloads.raspberrypi.org/raspbian_full_latest&lt;/A&gt; and follow the steps from &lt;SPAN style="font-size: 10.5pt;"&gt;&amp;nbsp;&lt;SPAN&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN11697.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN11697.pdf&lt;/A&gt; &lt;/SPAN&gt;&lt;/SPAN&gt;, the result is fine. Please kindly refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/64534iB273A22C2C25C465/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Apr 2019 09:37:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM5577-PN7120S-compatability-with-Raspberry-Pi-3-B/m-p/903952#M5429</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-04-28T09:37:44Z</dc:date>
    </item>
  </channel>
</rss>