<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Re: NT3H2111 Is there difference in readrange powered from RF-field or host</title>
    <link>https://community.nxp.com/t5/NFC/NT3H2111-Is-there-difference-in-readrange-powered-from-RF-field/m-p/879932#M5110</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear&amp;nbsp;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="226594" data-username="arnodegroot" href="https://community.nxp.com/people/arnodegroot"&gt;Arno de Groot&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;There should not be any difference in the read range, this device is still a passive element, so the read range&amp;nbsp; is the same for both cases, the section you refer here&amp;nbsp; talks about the arbitration of the EEPROM&amp;nbsp; in case that the RF interface try to&amp;nbsp; write or read from the EEPROM at the same time as the I2C interface. there is an arbitration to avoid this kind of collision.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Mar 2019 15:18:24 GMT</pubDate>
    <dc:creator>Jonathan_Iglesias</dc:creator>
    <dc:date>2019-03-28T15:18:24Z</dc:date>
    <item>
      <title>NT3H2111 Is there difference in readrange powered from RF-field or host</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-Is-there-difference-in-readrange-powered-from-RF-field/m-p/879931#M5109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We use the NT3H2111 without energy harvesting, so nothing is connected to the Vout pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any difference in readrange when the chip is: powered from RF-field first (without applying external power from the host), or when the chip is powered from the host first and then brought into the RF-field?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #007089; font-family: Arial-BoldMT; font-size: large;"&gt;11 Communication and arbitration between NFC and I&lt;/SPAN&gt;&lt;SPAN style="color: #007089; font-family: Arial-BoldMT; font-size: medium;"&gt;2&lt;/SPAN&gt;&lt;SPAN style="color: #007089; font-family: Arial-BoldMT; font-size: large;"&gt;C interface&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;"If both interfaces are powered by their corresponding source, only one interface shall&lt;/P&gt;&lt;P&gt;have access to the memory according to the "first-come, first-serve" principle."&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Mar 2019 08:18:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-Is-there-difference-in-readrange-powered-from-RF-field/m-p/879931#M5109</guid>
      <dc:creator>arnodegroot</dc:creator>
      <dc:date>2019-03-22T08:18:21Z</dc:date>
    </item>
    <item>
      <title>Re: NT3H2111 Is there difference in readrange powered from RF-field or host</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-Is-there-difference-in-readrange-powered-from-RF-field/m-p/879932#M5110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear&amp;nbsp;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="226594" data-username="arnodegroot" href="https://community.nxp.com/people/arnodegroot"&gt;Arno de Groot&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;There should not be any difference in the read range, this device is still a passive element, so the read range&amp;nbsp; is the same for both cases, the section you refer here&amp;nbsp; talks about the arbitration of the EEPROM&amp;nbsp; in case that the RF interface try to&amp;nbsp; write or read from the EEPROM at the same time as the I2C interface. there is an arbitration to avoid this kind of collision.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2019 15:18:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-Is-there-difference-in-readrange-powered-from-RF-field/m-p/879932#M5110</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2019-03-28T15:18:24Z</dc:date>
    </item>
  </channel>
</rss>