<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 pn7150 - multi node in one linux application</title>
    <link>https://community.nxp.com/t5/NFC/pn7150-multi-node-in-one-linux-application/m-p/879875#M5107</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;We have application which use 3 readers PN5xx with library "libnfc" in uart interface.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Now we want upgrade this solution with the support of ISO15693. So we have identified the PN7150.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our problem is the "linux_libnfc-nci" provided by NXP. Normaly it's compatible with i2C-dev driver kernel but we can't instanciate multi node with this library (many static and hard coded). Have you solution to use your library with 3 readers without rewrite all library?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have you another component with this standard with a library where we can instantiate multi readers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you :smileywink:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Apr 2019 14:04:26 GMT</pubDate>
    <dc:creator>thomas_villeboe</dc:creator>
    <dc:date>2019-04-04T14:04:26Z</dc:date>
    <item>
      <title>pn7150 - multi node in one linux application</title>
      <link>https://community.nxp.com/t5/NFC/pn7150-multi-node-in-one-linux-application/m-p/879875#M5107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;We have application which use 3 readers PN5xx with library "libnfc" in uart interface.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Now we want upgrade this solution with the support of ISO15693. So we have identified the PN7150.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our problem is the "linux_libnfc-nci" provided by NXP. Normaly it's compatible with i2C-dev driver kernel but we can't instanciate multi node with this library (many static and hard coded). Have you solution to use your library with 3 readers without rewrite all library?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have you another component with this standard with a library where we can instantiate multi readers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you :smileywink:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2019 14:04:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/pn7150-multi-node-in-one-linux-application/m-p/879875#M5107</guid>
      <dc:creator>thomas_villeboe</dc:creator>
      <dc:date>2019-04-04T14:04:26Z</dc:date>
    </item>
    <item>
      <title>Re: pn7150 - multi node in one linux application</title>
      <link>https://community.nxp.com/t5/NFC/pn7150-multi-node-in-one-linux-application/m-p/879876#M5108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;&lt;SPAN lang="EN-US"&gt;&lt;SPAN style="font-size: medium; font-family: Calibri; "&gt;Basically, you&amp;nbsp;can install&amp;nbsp;3 pn5xx-i2c kernel driver assigned to different I2C address (and different GPIOs) if the source code is updated to mount them with&amp;nbsp;3 different names (usually /dev/pn544, could be /dev/pn544_1, /dev/pn544_2 and /dev/pn544_3&amp;nbsp;for instance. ).&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;&lt;SPAN lang="EN-US"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;&lt;SPAN style="font-size: medium; font-family: Calibri; "&gt;Then the library can be modified to connect to the appropriate device node (then there will be&amp;nbsp;3 instance of the library).&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2019 08:34:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/pn7150-multi-node-in-one-linux-application/m-p/879876#M5108</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2019-04-09T08:34:47Z</dc:date>
    </item>
  </channel>
</rss>