<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Help with Active Load Modulation , PN5180 in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Help-with-Active-Load-Modulation-PN5180/m-p/879488#M5106</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Active Load Modulation is mainly meant to be used for smaller PICC antennas in card operation to overcome the minimum antenna size limitation to achieve standard conformance with Passive Load Modulation (PLM).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A greater range might be accomplished with a better antenna design mainly on the reader's side. The performance on mobile phones varies due to many factors such as metal enclosures and different antenna designs. It would be helpful to refer to PN5180's antenna design guide:&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN11740.pdf" title="https://www.nxp.com/docs/en/application-note/AN11740.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN11740.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Feb 2019 17:09:42 GMT</pubDate>
    <dc:creator>IvanRuiz</dc:creator>
    <dc:date>2019-02-22T17:09:42Z</dc:date>
    <item>
      <title>Help with Active Load Modulation , PN5180</title>
      <link>https://community.nxp.com/t5/NFC/Help-with-Active-Load-Modulation-PN5180/m-p/879487#M5105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sir,&lt;/P&gt;&lt;P&gt;I am testing the NFC distance emulating card tag ,with the evualuation board (PN5180 + LCP-Link2)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To simulate the card, i have use the example(NfcrdlibEx8_HCE_T4T) from NXP web.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I only can get a distance about 1cm, i want to increase it using the ALM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To increase this i have modified the value of some register from "phhalHw_Pn5180.h" but without&amp;nbsp;no results.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is any example or recomendation get more distance?&lt;/P&gt;&lt;P&gt;I need help, i am lost in this topic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 15:35:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Help-with-Active-Load-Modulation-PN5180/m-p/879487#M5105</guid>
      <dc:creator>clay_nurdk</dc:creator>
      <dc:date>2019-01-16T15:35:26Z</dc:date>
    </item>
    <item>
      <title>Re: Help with Active Load Modulation , PN5180</title>
      <link>https://community.nxp.com/t5/NFC/Help-with-Active-Load-Modulation-PN5180/m-p/879488#M5106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Active Load Modulation is mainly meant to be used for smaller PICC antennas in card operation to overcome the minimum antenna size limitation to achieve standard conformance with Passive Load Modulation (PLM).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A greater range might be accomplished with a better antenna design mainly on the reader's side. The performance on mobile phones varies due to many factors such as metal enclosures and different antenna designs. It would be helpful to refer to PN5180's antenna design guide:&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN11740.pdf" title="https://www.nxp.com/docs/en/application-note/AN11740.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN11740.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Feb 2019 17:09:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Help-with-Active-Load-Modulation-PN5180/m-p/879488#M5106</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2019-02-22T17:09:42Z</dc:date>
    </item>
  </channel>
</rss>