<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックCRLC663: general purpose output functionality</title>
    <link>https://community.nxp.com/t5/NFC/CRLC663-general-purpose-output-functionality/m-p/870408#M4979</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We would like to make use of the additional general purpose outputs of the CRLC663 chip in a future project to save pins on a MCU.&amp;nbsp; We would like to use the Pins OUT0 to OUT3 which are usually for the boundary scan.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've not found any information about the hardware functionality of the pins in the datasheet. The critical informations would be if the pins are either "voltage out" (like a MCU) or "sink" (eg. open drain) and how much current can be used per pin and in common. I know that some devices can provide like 5mA per port, but for example only 15mA in sum of all pins. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We aim to use 4 LED's which have 1-3mA per LED.&lt;/P&gt;&lt;P&gt;Also it would be interesting how the outputs react when the device is in reset or sleep mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for any information.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Feb 2019 08:14:19 GMT</pubDate>
    <dc:creator>jof</dc:creator>
    <dc:date>2019-02-18T08:14:19Z</dc:date>
    <item>
      <title>CRLC663: general purpose output functionality</title>
      <link>https://community.nxp.com/t5/NFC/CRLC663-general-purpose-output-functionality/m-p/870408#M4979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We would like to make use of the additional general purpose outputs of the CRLC663 chip in a future project to save pins on a MCU.&amp;nbsp; We would like to use the Pins OUT0 to OUT3 which are usually for the boundary scan.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've not found any information about the hardware functionality of the pins in the datasheet. The critical informations would be if the pins are either "voltage out" (like a MCU) or "sink" (eg. open drain) and how much current can be used per pin and in common. I know that some devices can provide like 5mA per port, but for example only 15mA in sum of all pins. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We aim to use 4 LED's which have 1-3mA per LED.&lt;/P&gt;&lt;P&gt;Also it would be interesting how the outputs react when the device is in reset or sleep mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for any information.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Feb 2019 08:14:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CRLC663-general-purpose-output-functionality/m-p/870408#M4979</guid>
      <dc:creator>jof</dc:creator>
      <dc:date>2019-02-18T08:14:19Z</dc:date>
    </item>
    <item>
      <title>Re: CRLC663: general purpose output functionality</title>
      <link>https://community.nxp.com/t5/NFC/CRLC663-general-purpose-output-functionality/m-p/870409#M4980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="315258" data-username="jof" href="https://community.nxp.com/people/jof"&gt;Jonathan &lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; OUT0~OUT7 all can be used as GPIO function. But these pins are multiplexed. You should do 2 steps for GPIO:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1. Enable them on corresponding bit in Register "PinEn"&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/72415iD5102F5E4A0B61BE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/72454iCC8E9941B4C729F5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;[note]&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can try to write 1 at bit0, and check if GPO function is enabled, otherwise write 0, please! I also didn't find detailed description on 1 or 0 for GPO function.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2. Output High Or Low&amp;nbsp; in Register "8.15.2 PinOut"&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/72484i91B02AA4242CBF0D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/72537iF5C8702148C9FAA2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Write 1 on related bit, High level should be output, otherwise Low level.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;In addtion, if your LED needs 1-3mA,&amp;nbsp; it is no problem to driver them diretly via GPO.&amp;nbsp; if higher current is needed, you can add a MOSFET to driver LEDs.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Have a nice day!&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Best Regards,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Weidong Sun&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2019 06:55:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CRLC663-general-purpose-output-functionality/m-p/870409#M4980</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2019-02-19T06:55:21Z</dc:date>
    </item>
  </channel>
</rss>