<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: Problems connecting to CLEV6640B</title>
    <link>https://community.nxp.com/t5/NFC/Problems-connecting-to-CLEV6640B/m-p/868366#M4952</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is a firmware update guide for PNEV5180, but can also apply for CLEV6630B, please kindly refer to &lt;A href="https://community.nxp.com/docs/DOC-334997"&gt;Program the firmware to PNEV5180B board&lt;/A&gt; for details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Mar 2019 06:50:35 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2019-03-19T06:50:35Z</dc:date>
    <item>
      <title>Problems connecting to CLEV6640B</title>
      <link>https://community.nxp.com/t5/NFC/Problems-connecting-to-CLEV6640B/m-p/868365#M4951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have problems connecting to my CLEV6640B board. It used to work, but no longer. Not sure what has happened with it since, it asked me about firmware updates when connecting it to NXP NFC Cockpit which I gave it and now it no longer wants to talk with the application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following is printed in the application when I connect to the port:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'courier new', courier, monospace; font-size: 13px;"&gt;[2019.03.18 16:12:15]:INFO:ServiceFactory:Generating Services for VCOM_RC663 @\\.\COM13&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'courier new', courier, monospace; font-size: 13px;"&gt;[2019.03.18 16:12:16]:ERROR:ServiceFactory:halRc663.ApplyProtocolSettings() Failed. Status=HAL,BUFFER_OVERFLOW&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'courier new', courier, monospace; font-size: 13px;"&gt;[2019.03.18 16:12:16]:ERROR:ServiceFactory:m_bal.SetConfig(HalHwType,RC663) failed. Status=HAL,BUFFER_OVERFLOW&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'courier new', courier, monospace; font-size: 13px;"&gt;[2019.03.18 16:12:16]:ERROR:ServiceFactory:generateServices(VCOM_RC663 @\\.\COM13) Failed with HAL,BUFFER_OVERFLOW&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'courier new', courier, monospace; font-size: 13px;"&gt;[2019.03.18 16:12:16]:INFO:ServiceFactory:uC FW Version: NNC_uC_VCOM_03.04.00_20180420 (Compiled on Apr 20 2018 19:05:55)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'courier new', courier, monospace; font-size: 13px;"&gt;[2019.03.18 16:12:16]:ERROR:ServiceFactory:SelectBalHalOsal(selected_board) Failed with HAL,BUFFER_OVERFLOW&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When connecting a scope on the SPI lines between the LPC and the CLRC663, it seems that he CLRC663 is communicating with the LPC. I did not decode the communication however to make sure the commands made sense.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I reflashed the LPC code using the&amp;nbsp;firmware&amp;nbsp;BootLoader_And_Nfcrdlib_SimplifiedAPI_EMVCo_Secondary.bin from NXP NFC Cockpit v4.8.0 but it did not help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I verified that NXP NFC Cockpit v4.8.0 could communicate with a card (thus ruling out issues with the USB drivers) using another CLEV6640B board and it worked without any problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This leaves the CLRC663 as a possible failure source. Is there any way I can reprogram the CLRC663 if this is the case?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Mar 2019 15:51:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Problems-connecting-to-CLEV6640B/m-p/868365#M4951</guid>
      <dc:creator>fredrik_jagenhe</dc:creator>
      <dc:date>2019-03-18T15:51:01Z</dc:date>
    </item>
    <item>
      <title>Re: Problems connecting to CLEV6640B</title>
      <link>https://community.nxp.com/t5/NFC/Problems-connecting-to-CLEV6640B/m-p/868366#M4952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is a firmware update guide for PNEV5180, but can also apply for CLEV6630B, please kindly refer to &lt;A href="https://community.nxp.com/docs/DOC-334997"&gt;Program the firmware to PNEV5180B board&lt;/A&gt; for details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2019 06:50:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Problems-connecting-to-CLEV6640B/m-p/868366#M4952</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-03-19T06:50:35Z</dc:date>
    </item>
  </channel>
</rss>