<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NHS3100 Temperature sensor in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NHS3100-Temperature-sensor/m-p/857826#M4810</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The exact location of the temperature sensor in the IC is not relevant; the bottom side has the largest thermal conductance. Temperature changes will be picked up quicker via the bottom - but the top side surely also contributes significantly! The graph you posted is not unexpected: the material used for the encasing and the amount of air surrounding the IC influence this behavior&amp;nbsp;a lot.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am assuming you are using the HVQFN24 IC, mounted on a PCB. A&amp;nbsp;typical PCB is not an efficient conductor of heat. Regarding the package, both the WLCSP25 and the W8 package will behave better in this regard. You can also&amp;nbsp;try to use another type of glue or physical connector to&amp;nbsp;better guide the heat towards the IC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the graph I don't get to see a timeline - I don't know your measurement interval. There is no point in optimizing beyond the needs of your use case - perhaps the slower temperature acceptance is acceptable after a few tweaks in your material?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can search around for thermal conductivity in general; there are also specialized firms that can provide you with professional support in this - I'm not a physicist nor a material expert (far from it!).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Good luck,&lt;/P&gt;&lt;P&gt;Dries.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Mar 2019 20:05:46 GMT</pubDate>
    <dc:creator>driesmoors</dc:creator>
    <dc:date>2019-03-15T20:05:46Z</dc:date>
    <item>
      <title>NHS3100 Temperature sensor</title>
      <link>https://community.nxp.com/t5/NFC/NHS3100-Temperature-sensor/m-p/857825#M4809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;dear all&lt;/P&gt;&lt;P&gt;I want to know how the NHS3100 temperature sensor work ?I means it get the environment temperature by packet below or bottom?&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74669i30F7D5D7CCBCFFA4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Because when I use the NHS3100,I use a box enclose the NHS3100.&lt;/P&gt;&lt;P&gt;just like this :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74816i3442C4417C004941/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;but I found that ,if I use the box ,the nhs3100 detect the temperature and change slowly than the 3100 without box .&lt;/P&gt;&lt;P&gt;the result like this :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74888i0333F6836CF28981/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so ,is there any suggestion for me when I use the box ?and I also want to know how the 3100 detect the temperature change ,from the packet top side or the bottom group pad ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I look forward to hearing from you。&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Mar 2019 08:22:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NHS3100-Temperature-sensor/m-p/857825#M4809</guid>
      <dc:creator>xiangxuejiao00</dc:creator>
      <dc:date>2019-03-14T08:22:21Z</dc:date>
    </item>
    <item>
      <title>Re: NHS3100 Temperature sensor</title>
      <link>https://community.nxp.com/t5/NFC/NHS3100-Temperature-sensor/m-p/857826#M4810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The exact location of the temperature sensor in the IC is not relevant; the bottom side has the largest thermal conductance. Temperature changes will be picked up quicker via the bottom - but the top side surely also contributes significantly! The graph you posted is not unexpected: the material used for the encasing and the amount of air surrounding the IC influence this behavior&amp;nbsp;a lot.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am assuming you are using the HVQFN24 IC, mounted on a PCB. A&amp;nbsp;typical PCB is not an efficient conductor of heat. Regarding the package, both the WLCSP25 and the W8 package will behave better in this regard. You can also&amp;nbsp;try to use another type of glue or physical connector to&amp;nbsp;better guide the heat towards the IC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the graph I don't get to see a timeline - I don't know your measurement interval. There is no point in optimizing beyond the needs of your use case - perhaps the slower temperature acceptance is acceptable after a few tweaks in your material?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can search around for thermal conductivity in general; there are also specialized firms that can provide you with professional support in this - I'm not a physicist nor a material expert (far from it!).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Good luck,&lt;/P&gt;&lt;P&gt;Dries.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Mar 2019 20:05:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NHS3100-Temperature-sensor/m-p/857826#M4810</guid>
      <dc:creator>driesmoors</dc:creator>
      <dc:date>2019-03-15T20:05:46Z</dc:date>
    </item>
  </channel>
</rss>