<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: OM5577: &amp;quot;NfcService Init Failed&amp;quot; after updating Raspberry Pi 3</title>
    <link>https://community.nxp.com/t5/NFC/OM5577-quot-NfcService-Init-Failed-quot-after-updating-Raspberry/m-p/562836#M479</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steven，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The image has some custom configuration that needed by the demo app, so it is not recommended installing updates based on that, but if you have to update the Pi, you might have to upgrade it manually, for example, update the packages that you want, and better leave the kernel as it is.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan Li&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Aug 2016 07:42:14 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2016-08-15T07:42:14Z</dc:date>
    <item>
      <title>OM5577: "NfcService Init Failed" after updating Raspberry Pi 3</title>
      <link>https://community.nxp.com/t5/NFC/OM5577-quot-NfcService-Init-Failed-quot-after-updating-Raspberry/m-p/562835#M478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recently installed the OM5577 Raspberry Pi Linux demo image (REV 1.2) onto an SD card for my Raspberry Pi 3. After starting up my Raspberry Pi 3, I confirmed that the OM5577 device was working by using the &lt;EM&gt;nfcDemoApp&lt;/EM&gt;. I then decided to check for updates for my Raspberry Pi using &lt;EM&gt;apt-get update&lt;/EM&gt; and then &lt;EM&gt;apt-get upgrade&lt;/EM&gt;. The following changes were made:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/944i4E14894D75EB21B9/image-size/large?v=v2&amp;amp;px=999" title="pic.jpg" alt="pic.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Right after doing the updates, I confirmed that the OM5577 device was still working using the &lt;EM&gt;nfcDemoApp&lt;/EM&gt;; however, after restarting my Raspberry Pi, I get the following error message when running the &lt;EM&gt;nfcDemoApp&lt;/EM&gt;:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;NfcService Init Failed&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm guessing that when installing the updates for the Raspberry Pi, a package that the &lt;EM&gt;nfcDemoApp&lt;/EM&gt; uses was either modified or removed. Does anyone know how I can fix this issue and get the &lt;EM&gt;nfcDemoApp&lt;/EM&gt; working again? I know that reinstalling the demo image will make it work, but I would rather be able to keep my Pi updated and still be able to use the OM5577 device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Steven T. Cacner, Jr.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Aug 2016 14:54:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM5577-quot-NfcService-Init-Failed-quot-after-updating-Raspberry/m-p/562835#M478</guid>
      <dc:creator>cacstech</dc:creator>
      <dc:date>2016-08-02T14:54:57Z</dc:date>
    </item>
    <item>
      <title>Re: OM5577: "NfcService Init Failed" after updating Raspberry Pi 3</title>
      <link>https://community.nxp.com/t5/NFC/OM5577-quot-NfcService-Init-Failed-quot-after-updating-Raspberry/m-p/562836#M479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steven，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The image has some custom configuration that needed by the demo app, so it is not recommended installing updates based on that, but if you have to update the Pi, you might have to upgrade it manually, for example, update the packages that you want, and better leave the kernel as it is.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan Li&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Aug 2016 07:42:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM5577-quot-NfcService-Init-Failed-quot-after-updating-Raspberry/m-p/562836#M479</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2016-08-15T07:42:14Z</dc:date>
    </item>
  </channel>
</rss>