<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックHow can you Flash (Not Debug) the NFC Library onto a CLRC663?</title>
    <link>https://community.nxp.com/t5/NFC/How-can-you-Flash-Not-Debug-the-NFC-Library-onto-a-CLRC663/m-p/854928#M4785</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I flash an example from the nfc library onto the NFC chip, the chip wont execute the program. When I debug, the program works after I execute via the start button. I believe it is something in the initialization, but I don't know where.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Feb 2019 19:28:41 GMT</pubDate>
    <dc:creator>joseph_kielasa</dc:creator>
    <dc:date>2019-02-11T19:28:41Z</dc:date>
    <item>
      <title>How can you Flash (Not Debug) the NFC Library onto a CLRC663?</title>
      <link>https://community.nxp.com/t5/NFC/How-can-you-Flash-Not-Debug-the-NFC-Library-onto-a-CLRC663/m-p/854928#M4785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I flash an example from the nfc library onto the NFC chip, the chip wont execute the program. When I debug, the program works after I execute via the start button. I believe it is something in the initialization, but I don't know where.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Feb 2019 19:28:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/How-can-you-Flash-Not-Debug-the-NFC-Library-onto-a-CLRC663/m-p/854928#M4785</guid>
      <dc:creator>joseph_kielasa</dc:creator>
      <dc:date>2019-02-11T19:28:41Z</dc:date>
    </item>
    <item>
      <title>Re: How can you Flash (Not Debug) the NFC Library onto a CLRC663?</title>
      <link>https://community.nxp.com/t5/NFC/How-can-you-Flash-Not-Debug-the-NFC-Library-onto-a-CLRC663/m-p/854929#M4786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe there is a confusion here with the reader's types.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Programmable NFC Controller:&lt;/STRONG&gt;&amp;nbsp;These highly integrated devices combine an NFC frontend with a freely programmable 32-bit Arm®&amp;nbsp;Cortex®-M0 microcontroller. They are the optimal solution for very compact footprints and function as your main system microcontroller.&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;NFC controller with integrated firmware:&lt;/STRONG&gt;&amp;nbsp;These plug-and-play solutions combine an NFC frontend with a 32-bit Cortex®-M0 microcontroller equipped with integrated firmware, and are optimized for use with application processors. They come with Linux™, Android™, and WinIoT drivers, and include an NCI interface.&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;NFC Frontend:&amp;nbsp;&lt;/STRONG&gt;These NFC devices are the most flexible way to add NFC connectivity to a system. The NFC stack runs on the separate system MCU. All our NFC frontends are supported by our NFC Reader Library, so design-in is fast and easy.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case the CLRC663 it's an NFC Frontend, so the stack can't be on the device as it should have a host MCU to send the different commands to the CLRC663.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have further questions, just let me know.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;Estephania&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 17:35:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/How-can-you-Flash-Not-Debug-the-NFC-Library-onto-a-CLRC663/m-p/854929#M4786</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-02-12T17:35:19Z</dc:date>
    </item>
  </channel>
</rss>