<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックCan't write 888 bytes to card using &amp;quot;explorenfc-basic write command&amp;quot;</title>
    <link>https://community.nxp.com/t5/NFC/Can-t-write-888-bytes-to-card-using-quot-explorenfc-basic-write/m-p/848417#M4703</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the "explore-nfc-ww" card to a raspberry pi and everything else works OK except writing to the card.&lt;/P&gt;&lt;P&gt;I can write 248 bytes with the "explorenfc-basic" write command, but the example rfid-card in the package is 888 bytes (NTAG216).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's not my card that is the problem because I developed a python program where I looped through every user area block (4 bytes in each block) and it worked up to 880 byte (using nxppy). But the python wrapper is not working perfect and I get error now and then. So I'm back into programming using C and the "basic.c" example in "neard-explorenfc_1.2.orig.tar. But this is the same as "explorenfc-basic"... with the writing problem...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is probably the problem explained:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://stackoverflow.com/questions/32203485/phone-recognize-nfc-tag-wrong-after-writing-with-raspberry" title="https://stackoverflow.com/questions/32203485/phone-recognize-nfc-tag-wrong-after-writing-with-raspberry"&gt;android - Phone recognize NFC tag wrong after writing with Raspberry - Stack Overflow&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an easy solution to get this working?&lt;/P&gt;&lt;P&gt;I want to read text, write text and read out the UID, not going to the moon...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Oct 2018 18:16:12 GMT</pubDate>
    <dc:creator>gruber1</dc:creator>
    <dc:date>2018-10-10T18:16:12Z</dc:date>
    <item>
      <title>Can't write 888 bytes to card using "explorenfc-basic write command"</title>
      <link>https://community.nxp.com/t5/NFC/Can-t-write-888-bytes-to-card-using-quot-explorenfc-basic-write/m-p/848417#M4703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the "explore-nfc-ww" card to a raspberry pi and everything else works OK except writing to the card.&lt;/P&gt;&lt;P&gt;I can write 248 bytes with the "explorenfc-basic" write command, but the example rfid-card in the package is 888 bytes (NTAG216).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's not my card that is the problem because I developed a python program where I looped through every user area block (4 bytes in each block) and it worked up to 880 byte (using nxppy). But the python wrapper is not working perfect and I get error now and then. So I'm back into programming using C and the "basic.c" example in "neard-explorenfc_1.2.orig.tar. But this is the same as "explorenfc-basic"... with the writing problem...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is probably the problem explained:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://stackoverflow.com/questions/32203485/phone-recognize-nfc-tag-wrong-after-writing-with-raspberry" title="https://stackoverflow.com/questions/32203485/phone-recognize-nfc-tag-wrong-after-writing-with-raspberry"&gt;android - Phone recognize NFC tag wrong after writing with Raspberry - Stack Overflow&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an easy solution to get this working?&lt;/P&gt;&lt;P&gt;I want to read text, write text and read out the UID, not going to the moon...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Oct 2018 18:16:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Can-t-write-888-bytes-to-card-using-quot-explorenfc-basic-write/m-p/848417#M4703</guid>
      <dc:creator>gruber1</dc:creator>
      <dc:date>2018-10-10T18:16:12Z</dc:date>
    </item>
  </channel>
</rss>