<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックNeed Help to detect 3 NFC cards using CLRC663 plus</title>
    <link>https://community.nxp.com/t5/NFC/Need-Help-to-detect-3-NFC-cards-using-CLRC663-plus/m-p/844562#M4650</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using CLRC663 plus connected externally with the MCU over UART.&amp;nbsp;&amp;nbsp;Using this CLRC663 plus reader we can detect two nfc type 2 tags simultaneously. Our requirement is to detect 3 nfc type 2 tags simultaneously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When we are trying to detect 3 tags simultaneously, then we are getting 3 bytes of UID but our UID length is 7 bytes. After debugging more in code, we found that SAK length is coming 2 bytes after cascade level 1 which should be 1 byte only.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We didn't want to use NFC reader library as it is creating a complexity in code for our HOST micro-controller as well as we are facing so many problems while porting the library on our HOST micro-controller. We have developed function routines to detect card and able to detect 2 cards simultaneously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would highly appreciated if we could get support to detect 3 multi-cards simultaneously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hasmukh Prajapati&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 11 Aug 2018 13:21:39 GMT</pubDate>
    <dc:creator>hasmukhprajapat</dc:creator>
    <dc:date>2018-08-11T13:21:39Z</dc:date>
    <item>
      <title>Need Help to detect 3 NFC cards using CLRC663 plus</title>
      <link>https://community.nxp.com/t5/NFC/Need-Help-to-detect-3-NFC-cards-using-CLRC663-plus/m-p/844562#M4650</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using CLRC663 plus connected externally with the MCU over UART.&amp;nbsp;&amp;nbsp;Using this CLRC663 plus reader we can detect two nfc type 2 tags simultaneously. Our requirement is to detect 3 nfc type 2 tags simultaneously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When we are trying to detect 3 tags simultaneously, then we are getting 3 bytes of UID but our UID length is 7 bytes. After debugging more in code, we found that SAK length is coming 2 bytes after cascade level 1 which should be 1 byte only.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We didn't want to use NFC reader library as it is creating a complexity in code for our HOST micro-controller as well as we are facing so many problems while porting the library on our HOST micro-controller. We have developed function routines to detect card and able to detect 2 cards simultaneously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would highly appreciated if we could get support to detect 3 multi-cards simultaneously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hasmukh Prajapati&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Aug 2018 13:21:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Need-Help-to-detect-3-NFC-cards-using-CLRC663-plus/m-p/844562#M4650</guid>
      <dc:creator>hasmukhprajapat</dc:creator>
      <dc:date>2018-08-11T13:21:39Z</dc:date>
    </item>
  </channel>
</rss>