<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NTAG 413 using libnfc-nci in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NTAG-413-using-libnfc-nci/m-p/840495#M4597</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="333036" data-username="shaun_s_k_yu@ite.edu.sg" href="https://community.nxp.com/people/shaun_s_k_yu@ite.edu.sg"&gt;Shaun Yu&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Hope you are doing great, I believe there are no examples specific for&amp;nbsp; NTAG 413 DNA using the NCI libdary, I think you can use the APIs in the library to&amp;nbsp; interact with NTAG 413 DNA, I will check if there is any example done&amp;nbsp; that&amp;nbsp; is public that we can share, since NTAG 413 DNA have some features that are not public and secured under NDA,&amp;nbsp; in case there is any example we will have to check if there are something under NDA or not to&amp;nbsp; publish it here. I see that you have other thread,&amp;nbsp; would you like to be answered in this thread so we dont have the same discussion in both ?&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/492180"&gt;https://community.nxp.com/thread/492180&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Jan 2019 16:07:13 GMT</pubDate>
    <dc:creator>Jonathan_Iglesias</dc:creator>
    <dc:date>2019-01-17T16:07:13Z</dc:date>
    <item>
      <title>NTAG 413 using libnfc-nci</title>
      <link>https://community.nxp.com/t5/NFC/NTAG-413-using-libnfc-nci/m-p/840494#M4596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How to use the libnfc-nci library to configure the NTAG 413 tags? In particular, how to change the keys and the CC Fie settings? I can see a file rw_t4t.c inside the library source that provides many interfaces to read and write to the various aspects like NDEF and CC File. Is there any examples on how to use these features? Has anyone tested this before?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Dec 2018 07:50:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG-413-using-libnfc-nci/m-p/840494#M4596</guid>
      <dc:creator>shaun_s_k_yu</dc:creator>
      <dc:date>2018-12-28T07:50:48Z</dc:date>
    </item>
    <item>
      <title>Re: NTAG 413 using libnfc-nci</title>
      <link>https://community.nxp.com/t5/NFC/NTAG-413-using-libnfc-nci/m-p/840495#M4597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="333036" data-username="shaun_s_k_yu@ite.edu.sg" href="https://community.nxp.com/people/shaun_s_k_yu@ite.edu.sg"&gt;Shaun Yu&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Hope you are doing great, I believe there are no examples specific for&amp;nbsp; NTAG 413 DNA using the NCI libdary, I think you can use the APIs in the library to&amp;nbsp; interact with NTAG 413 DNA, I will check if there is any example done&amp;nbsp; that&amp;nbsp; is public that we can share, since NTAG 413 DNA have some features that are not public and secured under NDA,&amp;nbsp; in case there is any example we will have to check if there are something under NDA or not to&amp;nbsp; publish it here. I see that you have other thread,&amp;nbsp; would you like to be answered in this thread so we dont have the same discussion in both ?&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/492180"&gt;https://community.nxp.com/thread/492180&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2019 16:07:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG-413-using-libnfc-nci/m-p/840495#M4597</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2019-01-17T16:07:13Z</dc:date>
    </item>
    <item>
      <title>Re: NTAG 413 using libnfc-nci</title>
      <link>https://community.nxp.com/t5/NFC/NTAG-413-using-libnfc-nci/m-p/840496#M4598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sure. I appreciate it. Anyhow, I do have a NDA between&amp;nbsp;ITE and the NXP in Singapore. WIll that suffice?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2019 00:44:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG-413-using-libnfc-nci/m-p/840496#M4598</guid>
      <dc:creator>shaun_s_k_yu</dc:creator>
      <dc:date>2019-01-18T00:44:26Z</dc:date>
    </item>
  </channel>
</rss>