<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 PN7462 + SAM AV2</title>
    <link>https://community.nxp.com/t5/NFC/PN7462-SAM-AV2/m-p/835728#M4518</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Members &amp;amp; NXP Support,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We&amp;nbsp;want to integrate SAM AV2 ( in SAM form not chip ) with PN7462 with its native ISO7816 port ( not AUX port ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any reference or firmware&amp;nbsp;example?&lt;/P&gt;&lt;P&gt;What is the proper operation? X-mode or Non-X mode?&lt;/P&gt;&lt;P&gt;I need also mifare plus HAL for PN7462?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Oct 2018 13:25:29 GMT</pubDate>
    <dc:creator>mukadder</dc:creator>
    <dc:date>2018-10-25T13:25:29Z</dc:date>
    <item>
      <title>PN7462 + SAM AV2</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-SAM-AV2/m-p/835728#M4518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Members &amp;amp; NXP Support,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We&amp;nbsp;want to integrate SAM AV2 ( in SAM form not chip ) with PN7462 with its native ISO7816 port ( not AUX port ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any reference or firmware&amp;nbsp;example?&lt;/P&gt;&lt;P&gt;What is the proper operation? X-mode or Non-X mode?&lt;/P&gt;&lt;P&gt;I need also mifare plus HAL for PN7462?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Oct 2018 13:25:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-SAM-AV2/m-p/835728#M4518</guid>
      <dc:creator>mukadder</dc:creator>
      <dc:date>2018-10-25T13:25:29Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 + SAM AV2</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-SAM-AV2/m-p/835729#M4519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mukadder Ceyhan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the ref project for mifare plus based on the NFC reader library for PN7462, but would you please create a private ticket via the following link? I may send the source code to you thru this channel. Thanks for your patience!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://nxpcommunity.force.com/community/CommunityContextPage" title="http://nxpcommunity.force.com/community/CommunityContextPage"&gt;http://nxpcommunity.force.com/community/CommunityContextPage&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Oct 2018 03:08:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-SAM-AV2/m-p/835729#M4519</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2018-10-30T03:08:59Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 + SAM AV2</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-SAM-AV2/m-p/835730#M4520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For PN7462 + SAM AV2 reference, we &lt;SPAN style="font-size: 11.0pt;"&gt;have in AccessDoor EC example. (package from docstore)&lt;/SPAN&gt;, &lt;SPAN style="font-size: 11.0pt;"&gt;There is also UM on this example &lt;A href="https://www.nxp.com/docs/en/user-guide/UM10957.pdf"&gt;https://www.nxp.com/docs/en/user-guide/UM10957.pdf.&lt;/A&gt;&amp;nbsp; It is non X mode, so DESFire authentications is performed by SAM module itself (PN is gateway iso7816 &amp;lt;-&amp;gt; ISO14443) . &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;You may download the following EC package from the docstore, please refer to the attachment for more details.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/66826i77F8B5ED5A622890/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Hope that helps,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Oct 2018 07:56:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-SAM-AV2/m-p/835730#M4520</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2018-10-30T07:56:59Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 + SAM AV2</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-SAM-AV2/m-p/835731#M4521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Mr. Kan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes created a topic ( ticket ) with&amp;nbsp;Case 00186909.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Nov 2018 10:34:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-SAM-AV2/m-p/835731#M4521</guid>
      <dc:creator>mukadder</dc:creator>
      <dc:date>2018-11-03T10:34:59Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 + SAM AV2</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-SAM-AV2/m-p/835732#M4522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Mr. Kan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is it also possible to make same scebario with aux interface, i.e using TDA8026 or related IC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I mean using two different mifare plus cards with different auth. secure elements ( i.e SAM ) by two SAM slot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Nov 2018 10:40:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-SAM-AV2/m-p/835732#M4522</guid>
      <dc:creator>mukadder</dc:creator>
      <dc:date>2018-11-03T10:40:33Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 + SAM AV2</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-SAM-AV2/m-p/835733#M4523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it is possible, there is TDA8026 available on the OM27462 board, with additional 3 SAM slots.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2018 05:56:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-SAM-AV2/m-p/835733#M4523</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2018-11-06T05:56:33Z</dc:date>
    </item>
  </channel>
</rss>