<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックAbout NFC NXP Library (reader).</title>
    <link>https://community.nxp.com/t5/NFC/About-NFC-NXP-Library-reader/m-p/835577#M4503</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Hi, as a Python beginner, i have some questions about my project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Bought few times ago a NFC sensor :&amp;nbsp;&lt;A class="link-titled" href="https://www.element14.com/community/docs/DOC-71574" title="https://www.element14.com/community/docs/DOC-71574"&gt;https://www.element14.com/community/docs/DOC-71574&lt;/A&gt;&amp;nbsp;&amp;nbsp;that should work with my Raspberry Pi Zero W.&lt;/P&gt;&lt;P&gt;I'm programming on PyCharm on Windows 10 (yes, the library is for Linux, know it) before exporting it on the Pi. The problem is that i see on the "&lt;A href="https://www.nxp.com/docs/en/application-note/AN11802.pdf"&gt;Library Guide&lt;/A&gt;" that the sensor only works with PI 2/3. So, i want to know if i can keep my Pi Zero or if it's impossible ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Thanks for the answer all.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Oct 2018 07:09:27 GMT</pubDate>
    <dc:creator>moureton_etienn</dc:creator>
    <dc:date>2018-10-08T07:09:27Z</dc:date>
    <item>
      <title>About NFC NXP Library (reader).</title>
      <link>https://community.nxp.com/t5/NFC/About-NFC-NXP-Library-reader/m-p/835577#M4503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Hi, as a Python beginner, i have some questions about my project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Bought few times ago a NFC sensor :&amp;nbsp;&lt;A class="link-titled" href="https://www.element14.com/community/docs/DOC-71574" title="https://www.element14.com/community/docs/DOC-71574"&gt;https://www.element14.com/community/docs/DOC-71574&lt;/A&gt;&amp;nbsp;&amp;nbsp;that should work with my Raspberry Pi Zero W.&lt;/P&gt;&lt;P&gt;I'm programming on PyCharm on Windows 10 (yes, the library is for Linux, know it) before exporting it on the Pi. The problem is that i see on the "&lt;A href="https://www.nxp.com/docs/en/application-note/AN11802.pdf"&gt;Library Guide&lt;/A&gt;" that the sensor only works with PI 2/3. So, i want to know if i can keep my Pi Zero or if it's impossible ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Thanks for the answer all.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Oct 2018 07:09:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/About-NFC-NXP-Library-reader/m-p/835577#M4503</guid>
      <dc:creator>moureton_etienn</dc:creator>
      <dc:date>2018-10-08T07:09:27Z</dc:date>
    </item>
    <item>
      <title>Re: About NFC NXP Library (reader).</title>
      <link>https://community.nxp.com/t5/NFC/About-NFC-NXP-Library-reader/m-p/835578#M4504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There should be no hardware issue to use Zero W with the NFC sensor as Zero W has the same 40 pin interface definition, and AN11802 doesn't specify the platform version, so I think you may use Pi Zero with that board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Oct 2018 07:49:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/About-NFC-NXP-Library-reader/m-p/835578#M4504</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2018-10-11T07:49:45Z</dc:date>
    </item>
  </channel>
</rss>