<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: NFC Class 6 Antenna Design</title>
    <link>https://community.nxp.com/t5/NFC/NFC-Class-6-Antenna-Design/m-p/549359#M423</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David Crosby:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You might want to take a look to the &lt;STRONG&gt;NTAG Antenna Design Guide&lt;/STRONG&gt; ZIP package (which includes the &lt;STRONG&gt;AN11276&lt;/STRONG&gt; application note). The ZIP is available from the next link and it includes reference Class6 antennas:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/identification-and-security/nfc-and-reader-ics/connected-tag-solutions/ntag-ic-plus-nfc-forum-type-2-tag-compliant-ic-with-ic-interface:NT3H2111_2211?fpsp=1&amp;amp;tab=Documentation_Tab#nogo" title="http://www.nxp.com/products/identification-and-security/nfc-and-reader-ics/connected-tag-solutions/ntag-ic-plus-nfc-forum-type-2-tag-compliant-ic-with-ic-interface:NT3H2111_2211?fpsp=1&amp;amp;tab=Documentation_Tab#nogo"&gt;NTAG I2C plus |Connected NFC Tag with I2C Interface|NXP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically the same design should work either on PCB or in a Flexible material, as long as there a no metal surfaces in the surroundings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Jul 2016 02:40:05 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2016-07-22T02:40:05Z</dc:date>
    <item>
      <title>NFC Class 6 Antenna Design</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Class-6-Antenna-Design/m-p/549358#M422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Is there are reference design for a Class 6 antenna on standard 0.062" thick FR4 material? I have seen a Class 6 flex circuit reference design only.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2016 18:27:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Class-6-Antenna-Design/m-p/549358#M422</guid>
      <dc:creator>davidcrosby</dc:creator>
      <dc:date>2016-07-07T18:27:26Z</dc:date>
    </item>
    <item>
      <title>Re: NFC Class 6 Antenna Design</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Class-6-Antenna-Design/m-p/549359#M423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David Crosby:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You might want to take a look to the &lt;STRONG&gt;NTAG Antenna Design Guide&lt;/STRONG&gt; ZIP package (which includes the &lt;STRONG&gt;AN11276&lt;/STRONG&gt; application note). The ZIP is available from the next link and it includes reference Class6 antennas:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/identification-and-security/nfc-and-reader-ics/connected-tag-solutions/ntag-ic-plus-nfc-forum-type-2-tag-compliant-ic-with-ic-interface:NT3H2111_2211?fpsp=1&amp;amp;tab=Documentation_Tab#nogo" title="http://www.nxp.com/products/identification-and-security/nfc-and-reader-ics/connected-tag-solutions/ntag-ic-plus-nfc-forum-type-2-tag-compliant-ic-with-ic-interface:NT3H2111_2211?fpsp=1&amp;amp;tab=Documentation_Tab#nogo"&gt;NTAG I2C plus |Connected NFC Tag with I2C Interface|NXP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically the same design should work either on PCB or in a Flexible material, as long as there a no metal surfaces in the surroundings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jul 2016 02:40:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Class-6-Antenna-Design/m-p/549359#M423</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2016-07-22T02:40:05Z</dc:date>
    </item>
  </channel>
</rss>