<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Bit error count from MFRC531? in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Bit-error-count-from-MFRC531/m-p/544866#M412</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sorry, but MFR531 just supports parity and CRC error detection, do you mean bit collision detection? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan Li&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Aug 2016 07:41:27 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2016-08-04T07:41:27Z</dc:date>
    <item>
      <title>Bit error count from MFRC531?</title>
      <link>https://community.nxp.com/t5/NFC/Bit-error-count-from-MFRC531/m-p/544865#M411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any way I can get bit error count from MFRC531? It is to help me optimize read/write distance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2016 12:14:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Bit-error-count-from-MFRC531/m-p/544865#M411</guid>
      <dc:creator>deanfjellerad</dc:creator>
      <dc:date>2016-07-27T12:14:15Z</dc:date>
    </item>
    <item>
      <title>Re: Bit error count from MFRC531?</title>
      <link>https://community.nxp.com/t5/NFC/Bit-error-count-from-MFRC531/m-p/544866#M412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sorry, but MFR531 just supports parity and CRC error detection, do you mean bit collision detection? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan Li&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Aug 2016 07:41:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Bit-error-count-from-MFRC531/m-p/544866#M412</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2016-08-04T07:41:27Z</dc:date>
    </item>
    <item>
      <title>Re: Bit error count from MFRC531?</title>
      <link>https://community.nxp.com/t5/NFC/Bit-error-count-from-MFRC531/m-p/544867#M413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Ken&lt;/P&gt;&lt;P&gt;Thanks for reply.&lt;/P&gt;&lt;P&gt;the error reg does not seem to change much.&lt;/P&gt;&lt;P&gt;the closest i could get a error count is to use the s valid signal.&lt;/P&gt;&lt;P&gt;but it also have a very tight tolerance, making it almost useless for that job.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Aug 2016 09:14:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Bit-error-count-from-MFRC531/m-p/544867#M413</guid>
      <dc:creator>deanfjellerad</dc:creator>
      <dc:date>2016-08-04T09:14:41Z</dc:date>
    </item>
  </channel>
</rss>