<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 NHS3100 RTC</title>
    <link>https://community.nxp.com/t5/NFC/NHS3100-RTC/m-p/810141#M4117</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My customer used NHS3100 internal RTC with 32kHz FRO clock. There's considerable deviation for the RTC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At room temperature, the deviation is less than 10s per two days;&lt;/P&gt;&lt;P&gt;If placed two boards in the fridge, where the ambient temp is about -10~-20℃, the deviation between the two boards is about 20min per day. While with sw calibration, the deviation could be reduced to several minutes.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Customer questions are:&lt;/P&gt;&lt;P&gt;1. Do we have the accuracy characteristic of the internal 32kHz FRO clock/ RTC?&lt;/P&gt;&lt;P&gt;2. Do we have ANs or suggestions to improve the RTC accuracy of wide circumstance temp range?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Nov 2018 07:59:54 GMT</pubDate>
    <dc:creator>fantasy</dc:creator>
    <dc:date>2018-11-28T07:59:54Z</dc:date>
    <item>
      <title>NHS3100 RTC</title>
      <link>https://community.nxp.com/t5/NFC/NHS3100-RTC/m-p/810141#M4117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My customer used NHS3100 internal RTC with 32kHz FRO clock. There's considerable deviation for the RTC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At room temperature, the deviation is less than 10s per two days;&lt;/P&gt;&lt;P&gt;If placed two boards in the fridge, where the ambient temp is about -10~-20℃, the deviation between the two boards is about 20min per day. While with sw calibration, the deviation could be reduced to several minutes.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Customer questions are:&lt;/P&gt;&lt;P&gt;1. Do we have the accuracy characteristic of the internal 32kHz FRO clock/ RTC?&lt;/P&gt;&lt;P&gt;2. Do we have ANs or suggestions to improve the RTC accuracy of wide circumstance temp range?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Nov 2018 07:59:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NHS3100-RTC/m-p/810141#M4117</guid>
      <dc:creator>fantasy</dc:creator>
      <dc:date>2018-11-28T07:59:54Z</dc:date>
    </item>
    <item>
      <title>Re: NHS3100 RTC</title>
      <link>https://community.nxp.com/t5/NFC/NHS3100-RTC/m-p/810142#M4118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fantasy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you download the NHS3100 SDK(&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=RELEASE-MRA2-NHS3100-11_2&amp;amp;appType=license&amp;amp;Parent_nodeId=1447656128903712551836&amp;amp;Parent_pageType=product" title="https://www.nxp.com/webapp/Download?colCode=RELEASE-MRA2-NHS3100-11_2&amp;amp;appType=license&amp;amp;Parent_nodeId=1447656128903712551836&amp;amp;Parent_pageType=product"&gt;https://www.nxp.com/webapp/Download?colCode=RELEASE-MRA2-NHS3100-11_2&amp;amp;appType=license&amp;amp;Parent_nodeId=14476561289037125518…&lt;/A&gt;&amp;nbsp;), you may find the app note on this topic in that package. Please refer to the following for more details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_247.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78494i78C0078C1F2E9F5B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_247.png" alt="pastedImage_247.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Nov 2018 04:54:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NHS3100-RTC/m-p/810142#M4118</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2018-11-30T04:54:29Z</dc:date>
    </item>
  </channel>
</rss>