<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PN7462 Secondary Bootloader in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN7462-Secondary-Bootloader/m-p/803663#M4011</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could be please describe your procedure little bit more in detail? You've used re-directing vector table using the asm code provided in AN10995, modified linkerscripts (making another space for bootloader) generated for PN7462 example projects, and used phhalFlash for&amp;nbsp;controlling&amp;nbsp;internal flash memory? - this was procedure I was using for LPC11xx (with IAP procedure for controlling internal flash memory), but not sure if same approach should be used also here, since PN7462 has a lot of supporting functions.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks for detailed description.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Milan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 02 May 2020 09:22:22 GMT</pubDate>
    <dc:creator>m_sedlak</dc:creator>
    <dc:date>2020-05-02T09:22:22Z</dc:date>
    <item>
      <title>PN7462 Secondary Bootloader</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Secondary-Bootloader/m-p/803660#M4008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any possibility to write a SW bootloader ( via uart, i2c etc. ) on PN7462?&lt;/P&gt;&lt;P&gt;Or what is the proper way to &lt;STRONG&gt;&lt;EM&gt;remote update&lt;/EM&gt;&amp;nbsp;&lt;/STRONG&gt;its&amp;nbsp;firmware?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;P&gt;Mukadder.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2018 08:41:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Secondary-Bootloader/m-p/803660#M4008</guid>
      <dc:creator>mukadder</dc:creator>
      <dc:date>2018-11-06T08:41:34Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 Secondary Bootloader</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Secondary-Bootloader/m-p/803661#M4009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently you could only refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN10995.zip"&gt;AN10995&lt;/A&gt;. The secondary Bootloader project described here is implemented with the M0 LPC and many concepts could be reused also in PN7462AU project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Nov 2018 23:00:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Secondary-Bootloader/m-p/803661#M4009</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2018-11-13T23:00:59Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 Secondary Bootloader</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Secondary-Bootloader/m-p/803662#M4010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally finished the development successfully. It uses HSU /&amp;nbsp;VCOM with XMODEM protocol and also optionally uses NOR flash memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mukadder&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jun 2019 17:56:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Secondary-Bootloader/m-p/803662#M4010</guid>
      <dc:creator>mukadder</dc:creator>
      <dc:date>2019-06-27T17:56:12Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 Secondary Bootloader</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Secondary-Bootloader/m-p/803663#M4011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could be please describe your procedure little bit more in detail? You've used re-directing vector table using the asm code provided in AN10995, modified linkerscripts (making another space for bootloader) generated for PN7462 example projects, and used phhalFlash for&amp;nbsp;controlling&amp;nbsp;internal flash memory? - this was procedure I was using for LPC11xx (with IAP procedure for controlling internal flash memory), but not sure if same approach should be used also here, since PN7462 has a lot of supporting functions.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks for detailed description.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Milan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 May 2020 09:22:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Secondary-Bootloader/m-p/803663#M4011</guid>
      <dc:creator>m_sedlak</dc:creator>
      <dc:date>2020-05-02T09:22:22Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 Secondary Bootloader</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Secondary-Bootloader/m-p/803664#M4012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Milan,&lt;/P&gt;&lt;P&gt;Sorry to write late.&lt;/P&gt;&lt;P&gt;You can follow AN10995 but since there is no VTOR in this architecture you must re-map some vectors to the user space with a static variable which must be located at the bottom of the SRAM. I am not using IAR and implemented with Keil.&lt;/P&gt;&lt;P&gt;So; to start,&lt;/P&gt;&lt;P&gt;*&amp;nbsp; Reserve some additional bytes in SRAM ;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;//SRAM 1st 32 Byte is reserved: 0x100000 ... 0x100020 used by Vectors ( Reserved )&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;//SRAM 2nd 32 Byte is reserved: 0x100020 ... 0x100040 by Sw Bootloader&lt;/P&gt;&lt;P&gt;* Use IRQ mapping ( for example if application starts at 0x20B000UL ) Your ( if used in bootloader ) IRQ handlers must like;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void SysTick_Handler(void )&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;if( !irq_Handler_Get_Map() )&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;sysTickHandler(); &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Bootloader Side&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;else&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;app_SysTick_Handler();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // User Side&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;volatile int irqMap __attribute__((section(".ARM.__at_0x100020")));&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int irq_Handler_Get_Map( void )&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;return irqMap;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int irq_Handler_Set_Map( int map_Value )&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;irqMap = map_Value;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;return irqMap;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;* You can use the following Flash Memory Example;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int isp_Flash_WriteTest( void )&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;int i;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;unsigned long flashOffsetAddr = 32*1024;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;unsigned long dwPageNumber;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;uint8_t *ReadAddress;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;phStatus_t flashStatus;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;//WRITE START HERE&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;dwPageNumber = PHHAL_FLASH_USER_PAGE_START + flashOffsetAddr / PHHAL_FLASH_PAGE_SIZE;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;utilUartPrintf("Starting Flash-Write...Page: %d\n", dwPageNumber );&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;isp_Flash_Init();&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;for( i = 0; i&amp;lt;5; ++i )&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;memset( flashBuffer, 0xA0 + i, sizeof(flashBuffer) );&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;flashStatus = phhalFlash_WritePage( dwPageNumber + i, flashBuffer );&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;//READ START HERE...&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;ReadAddress = (unsigned char *) ( flashOffsetAddr + PHHAL_FLASH_USER_START_ADDRESS );&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;utilUartPrintf("Starting Flash-Read...%d\n", ReadAddress );&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;isp_Flash_Init();&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;for( i = 0; i&amp;lt;5; ++i )&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;ReadAddress = (unsigned char *) ( flashOffsetAddr + PHHAL_FLASH_USER_START_ADDRESS + i * PHHAL_FLASH_PAGE_SIZE );&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;flashStatus = phhalFlash_ReadBuffer( flashBuffer, ReadAddress, PHHAL_FLASH_PAGE_SIZE );&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;debugPrintHexDump("Buffer", flashBuffer, PHHAL_FLASH_PAGE_SIZE );&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;return 1;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 May 2020 09:53:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Secondary-Bootloader/m-p/803664#M4012</guid>
      <dc:creator>mukadder</dc:creator>
      <dc:date>2020-05-19T09:53:56Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 Secondary Bootloader</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Secondary-Bootloader/m-p/1268058#M8453</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/54009"&gt;@mukadder&lt;/a&gt;,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/166773"&gt;@IvanRuiz&lt;/a&gt;&amp;nbsp;&amp;amp;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/80068"&gt;@m_sedlak&lt;/a&gt;.&lt;BR /&gt;I am using the MCU Expresso IDE for the development of PN7462 NFC.&lt;BR /&gt;I would like to know the detailed procedure for implementing the secondary bootloader application to the&amp;nbsp;PN7462AU_ex_phExCcid example.&lt;BR /&gt;Will you please give me a reference related to it?&lt;/P&gt;</description>
      <pubDate>Mon, 26 Apr 2021 09:33:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Secondary-Bootloader/m-p/1268058#M8453</guid>
      <dc:creator>shiv_patil</dc:creator>
      <dc:date>2021-04-26T09:33:42Z</dc:date>
    </item>
  </channel>
</rss>