<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MFRC522 Multiple SPI in NFC</title>
    <link>https://community.nxp.com/t5/NFC/MFRC522-Multiple-SPI/m-p/799661#M3969</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/tag/MFRC522/tg-p"&gt;#MFRC522&lt;/A&gt;&amp;nbsp; Multi SPI&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;Connect SPI communication (MISO / MOSI / SCK / SS) with the microcomputer&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would like to do multi-control,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When multiple units are connected,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Even if you select the device you want to communicate with the SS terminal,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Other If the MISO port of the device is output "Low"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If the selected MISO output level goes down and the communication&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It will not be possible.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is MFRC 522 supported only 1: 1 SPI?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Jun 2018 00:52:58 GMT</pubDate>
    <dc:creator>kita</dc:creator>
    <dc:date>2018-06-20T00:52:58Z</dc:date>
    <item>
      <title>MFRC522 Multiple SPI</title>
      <link>https://community.nxp.com/t5/NFC/MFRC522-Multiple-SPI/m-p/799661#M3969</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/tag/MFRC522/tg-p"&gt;#MFRC522&lt;/A&gt;&amp;nbsp; Multi SPI&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;Connect SPI communication (MISO / MOSI / SCK / SS) with the microcomputer&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would like to do multi-control,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When multiple units are connected,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Even if you select the device you want to communicate with the SS terminal,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Other If the MISO port of the device is output "Low"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If the selected MISO output level goes down and the communication&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It will not be possible.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is MFRC 522 supported only 1: 1 SPI?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jun 2018 00:52:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MFRC522-Multiple-SPI/m-p/799661#M3969</guid>
      <dc:creator>kita</dc:creator>
      <dc:date>2018-06-20T00:52:58Z</dc:date>
    </item>
    <item>
      <title>Re: MFRC522 Multiple SPI</title>
      <link>https://community.nxp.com/t5/NFC/MFRC522-Multiple-SPI/m-p/799662#M3970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, MFRC522 supports only one SPI interface.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jun 2018 06:41:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MFRC522-Multiple-SPI/m-p/799662#M3970</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2018-06-25T06:41:56Z</dc:date>
    </item>
    <item>
      <title>Re: MFRC522 Multiple SPI</title>
      <link>https://community.nxp.com/t5/NFC/MFRC522-Multiple-SPI/m-p/799663#M3971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;Thank you for answering.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;◆When MFRC 522 is used in 1 (Master): N (Slave)&lt;BR /&gt;I plan to communicate by switching the SS terminal and MISO port to the device I want to communicate with.&lt;BR /&gt;Is there not a problem?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;※N (Slave) unit　MOSI / SCK / RST ports share.&lt;SPAN style="display: none;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;◆Does MFRC-630 support 1 (Master): N (Slave) communication?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;Kan_Li&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jun 2018 07:39:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MFRC522-Multiple-SPI/m-p/799663#M3971</guid>
      <dc:creator>kita</dc:creator>
      <dc:date>2018-06-25T07:39:46Z</dc:date>
    </item>
  </channel>
</rss>