<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックNTAG I2CPlus Problem</title>
    <link>https://community.nxp.com/t5/NFC/NTAG-I2CPlus-Problem/m-p/789905#M3878</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I´m developing a new board and we want to add to it a NXP NTAG I2CPlus device (NT3H2111) by the moment we only want read the device unique 7 bytes UID using I2C and with an external mobile phone using NFC, we don´t need by the moment communicate between mobile phone and our board, we only want that the mobile phone(using NFC) and the device on our board(using I2C) can read the same 7 bytes UID.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I can read with my microcontroller the UID using the I2C, but the NFC interface is not working, I can not read the UID of the Ntag using a mobile phone.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible from the NFC side to read the Ntag´s UID if we have not configured nothing from the I2c side?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The&amp;nbsp;&lt;SPAN&gt;NT3H2111 is powered from a 3.3V power supply&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I´ve attached a photo of the board with the antenna.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Oct 2018 09:29:16 GMT</pubDate>
    <dc:creator>manuelbuil</dc:creator>
    <dc:date>2018-10-31T09:29:16Z</dc:date>
    <item>
      <title>NTAG I2CPlus Problem</title>
      <link>https://community.nxp.com/t5/NFC/NTAG-I2CPlus-Problem/m-p/789905#M3878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I´m developing a new board and we want to add to it a NXP NTAG I2CPlus device (NT3H2111) by the moment we only want read the device unique 7 bytes UID using I2C and with an external mobile phone using NFC, we don´t need by the moment communicate between mobile phone and our board, we only want that the mobile phone(using NFC) and the device on our board(using I2C) can read the same 7 bytes UID.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I can read with my microcontroller the UID using the I2C, but the NFC interface is not working, I can not read the UID of the Ntag using a mobile phone.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible from the NFC side to read the Ntag´s UID if we have not configured nothing from the I2c side?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The&amp;nbsp;&lt;SPAN&gt;NT3H2111 is powered from a 3.3V power supply&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I´ve attached a photo of the board with the antenna.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Oct 2018 09:29:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG-I2CPlus-Problem/m-p/789905#M3878</guid>
      <dc:creator>manuelbuil</dc:creator>
      <dc:date>2018-10-31T09:29:16Z</dc:date>
    </item>
    <item>
      <title>Re: NTAG I2CPlus Problem</title>
      <link>https://community.nxp.com/t5/NFC/NTAG-I2CPlus-Problem/m-p/789906#M3879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the UID cannot even be read from the NFC Interface, it is most likely a Hardware problem. It would be helpful to refer to the Antenna Design Guide:&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN11276.zip" title="https://www.nxp.com/docs/en/application-note/AN11276.zip"&gt;https://www.nxp.com/docs/en/application-note/AN11276.zip&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Dec 2018 23:12:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG-I2CPlus-Problem/m-p/789906#M3879</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2018-12-27T23:12:41Z</dc:date>
    </item>
  </channel>
</rss>