<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 NCI version mismatch</title>
    <link>https://community.nxp.com/t5/NFC/NCI-version-mismatch/m-p/541175#M384</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our board has a PN7120 NFC controller on it.&amp;nbsp; I'm using Qualcomm's Android (Marshmallow on an 820) including vendor/nxp/opensource/external/libnfc-nci.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using an NFC application, the library receives a reset notification from the chip.&amp;nbsp; The reset indicates that the chip supports NCI version 0.&amp;nbsp; However, the library supports only NCI version src/include/nfc_target.h, the only two versions supported are 0x0F and 0x10 (defaults to 0x10).&amp;nbsp; This causes the NFC stack to fail to start:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NxpTml&amp;nbsp; : PN54X - I2C Read successful.....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NxpNciR : len =&amp;nbsp;&amp;nbsp; 9 &amp;gt; 600006A000C7D40000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NxpTml&amp;nbsp; : PN54X - Posting read message.....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NxpHal&amp;nbsp; : read successful status = 0x0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NxpHal&amp;nbsp; : CORE_RESET_NTF received!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NxpHal&amp;nbsp; : phNxpNciHal_emergency_recovery: abort()&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NfcAdaptation: NfcAdaptation::HalDeviceContextDataCallback: len=9&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BrcmNfcNfa: NFC received ntf gid:0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BrcmNfcNfa: nci_proc_core_ntf opcode:0x0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BrcmNfcNfa: reset notification!!:0xa0 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BrcmNfcNfa: NCI version mismatch!!:0x10 != 0x00 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BrcmNfcNfa: NFCC version is too old&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BrcmNfcNfa: Failed to reset NFCC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The application note &lt;A href="http://www.nxp.com/documents/application_note/AN11690.pdf" title="http://www.nxp.com/documents/application_note/AN11690.pdf"&gt;http://www.nxp.com/documents/application_note/AN11690.pdf&lt;/A&gt; describes how to use the PN7120 with Android.&amp;nbsp; It specifies github.com/NXPNFCLinux/linux_libnfc-nci as the source for the library.&amp;nbsp; Although it differs somewhat from libnfc-nci included in the Qualcomm Android BSP, it too supports NCI version 0x0F and 0x10.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone explain why the chip version seems old?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Steve&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Jul 2016 14:19:09 GMT</pubDate>
    <dc:creator>steveschefter</dc:creator>
    <dc:date>2016-07-05T14:19:09Z</dc:date>
    <item>
      <title>NCI version mismatch</title>
      <link>https://community.nxp.com/t5/NFC/NCI-version-mismatch/m-p/541175#M384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our board has a PN7120 NFC controller on it.&amp;nbsp; I'm using Qualcomm's Android (Marshmallow on an 820) including vendor/nxp/opensource/external/libnfc-nci.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using an NFC application, the library receives a reset notification from the chip.&amp;nbsp; The reset indicates that the chip supports NCI version 0.&amp;nbsp; However, the library supports only NCI version src/include/nfc_target.h, the only two versions supported are 0x0F and 0x10 (defaults to 0x10).&amp;nbsp; This causes the NFC stack to fail to start:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NxpTml&amp;nbsp; : PN54X - I2C Read successful.....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NxpNciR : len =&amp;nbsp;&amp;nbsp; 9 &amp;gt; 600006A000C7D40000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NxpTml&amp;nbsp; : PN54X - Posting read message.....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NxpHal&amp;nbsp; : read successful status = 0x0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NxpHal&amp;nbsp; : CORE_RESET_NTF received!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NxpHal&amp;nbsp; : phNxpNciHal_emergency_recovery: abort()&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NfcAdaptation: NfcAdaptation::HalDeviceContextDataCallback: len=9&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BrcmNfcNfa: NFC received ntf gid:0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BrcmNfcNfa: nci_proc_core_ntf opcode:0x0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BrcmNfcNfa: reset notification!!:0xa0 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BrcmNfcNfa: NCI version mismatch!!:0x10 != 0x00 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BrcmNfcNfa: NFCC version is too old&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BrcmNfcNfa: Failed to reset NFCC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The application note &lt;A href="http://www.nxp.com/documents/application_note/AN11690.pdf" title="http://www.nxp.com/documents/application_note/AN11690.pdf"&gt;http://www.nxp.com/documents/application_note/AN11690.pdf&lt;/A&gt; describes how to use the PN7120 with Android.&amp;nbsp; It specifies github.com/NXPNFCLinux/linux_libnfc-nci as the source for the library.&amp;nbsp; Although it differs somewhat from libnfc-nci included in the Qualcomm Android BSP, it too supports NCI version 0x0F and 0x10.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone explain why the chip version seems old?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Steve&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jul 2016 14:19:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NCI-version-mismatch/m-p/541175#M384</guid>
      <dc:creator>steveschefter</dc:creator>
      <dc:date>2016-07-05T14:19:09Z</dc:date>
    </item>
    <item>
      <title>Re: NCI version mismatch</title>
      <link>https://community.nxp.com/t5/NFC/NCI-version-mismatch/m-p/541176#M385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the Qualcomm NFC stack is developed to work with a different NFC IC (called NQ2xx). PN7120 is not supported by this stack.&lt;/P&gt;&lt;P&gt;If you want to use Android with PN7120, please follow the Android guide for PN7120, but then it is not based on Qualcomm's NFC Android stack.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jul 2016 02:55:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NCI-version-mismatch/m-p/541176#M385</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2016-07-18T02:55:06Z</dc:date>
    </item>
  </channel>
</rss>