<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: hello     Now I want to develop a project to use nt3h2111 NFC chip,      system general' working process is like this, there is a      card reader, and a controller in the system, card reader      and the controller  transmission instruction through t</title>
    <link>https://community.nxp.com/t5/NFC/NFC-MIRROR-FAILED/m-p/781079#M3801</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Nov 2017 06:50:15 GMT</pubDate>
    <dc:creator>sunxin</dc:creator>
    <dc:date>2017-11-17T06:50:15Z</dc:date>
    <item>
      <title>NFC MIRROR FAILED</title>
      <link>https://community.nxp.com/t5/NFC/NFC-MIRROR-FAILED/m-p/781078#M3800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello&lt;BR /&gt; Now I want to develop a project to use nt3h2111 NFC chip, &lt;BR /&gt; system general' working process is like this, there is a &lt;BR /&gt; card reader, and a controller in the system, card reader &lt;BR /&gt; and the controller transmission instruction through the &lt;BR /&gt; NFC ram, so will the ram address back to the mirror, &lt;BR /&gt; the reader can also read or write nfc ram, now the problem is &lt;BR /&gt; that when the card reader close to the NFC chip ,now controller &lt;BR /&gt; execution initialization for NFC, and sometimes I found that &lt;BR /&gt; the mirror will fail&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Nov 2017 06:48:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-MIRROR-FAILED/m-p/781078#M3800</guid>
      <dc:creator>sunxin</dc:creator>
      <dc:date>2017-11-17T06:48:48Z</dc:date>
    </item>
    <item>
      <title>Re: hello     Now I want to develop a project to use nt3h2111 NFC chip,      system general' working process is like this, there is a      card reader, and a controller in the system, card reader      and the controller  transmission instruction through t</title>
      <link>https://community.nxp.com/t5/NFC/NFC-MIRROR-FAILED/m-p/781079#M3801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Nov 2017 06:50:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-MIRROR-FAILED/m-p/781079#M3801</guid>
      <dc:creator>sunxin</dc:creator>
      <dc:date>2017-11-17T06:50:15Z</dc:date>
    </item>
    <item>
      <title>Re: hello     Now I want to develop a project to use nt3h2111 NFC chip,      system general' working process is like this, there is a      card reader, and a controller in the system, card reader      and the controller  transmission instruction through t</title>
      <link>https://community.nxp.com/t5/NFC/NFC-MIRROR-FAILED/m-p/781080#M3802</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;UL style="list-style-type: disc;"&gt;&lt;LI&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33594iE912E6D4796A7B4F/image-size/large?v=v2&amp;amp;px=999" title="{47A6EAD9-0B86-4476-A896-0B117205BF43&amp;amp;#125;.png" alt="{47A6EAD9-0B86-4476-A896-0B117205BF43&amp;amp;#125;.png" /&gt;&lt;/span&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Nov 2017 07:00:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-MIRROR-FAILED/m-p/781080#M3802</guid>
      <dc:creator>sunxin</dc:creator>
      <dc:date>2017-11-17T07:00:55Z</dc:date>
    </item>
    <item>
      <title>Re: NFC MIRROR FAILED</title>
      <link>https://community.nxp.com/t5/NFC/NFC-MIRROR-FAILED/m-p/781081#M3803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please make sure that you are enabling correctly the block to be mirrored. For instance, the data in SRAM cannot be mirrored to block 0 of the NTAG I2C EEPROM since it is the block which contains information of the Tag such as the UID which cannot be modified.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please mirror it starting from block number one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="token function"&gt;NTAG_SetSRAMMirrorOnOff&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;ntag_handle&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; true&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="token function"&gt;HAL_Timer_delay_ms&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;5&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="token function"&gt;NTAG_SetSRAMMirrorBlock&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;ntag_handle&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This way it allows me to see the SRAM reflected in EEPROM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Dec 2017 21:31:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-MIRROR-FAILED/m-p/781081#M3803</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2017-12-15T21:31:10Z</dc:date>
    </item>
    <item>
      <title>Re: NFC MIRROR FAILED</title>
      <link>https://community.nxp.com/t5/NFC/NFC-MIRROR-FAILED/m-p/781082#M3804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;oh！first ,thank you for replying my question very much.then,I have configurated the register SRAM_MIRROR_BLOCK as 0x30,it is not&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;block 0 of the NTAG I2C EEPROM,&lt;/SPAN&gt;and I have enabled the&amp;nbsp;&lt;SPAN&gt;SRAM_MIRROR,but &lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I found that &lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;the mirror will fail still.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f;"&gt;thanks for you help!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Dec 2017 09:07:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-MIRROR-FAILED/m-p/781082#M3804</guid>
      <dc:creator>sunxin</dc:creator>
      <dc:date>2017-12-20T09:07:16Z</dc:date>
    </item>
  </channel>
</rss>