<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 NTAG 216 - ISO 14443 - part 4</title>
    <link>https://community.nxp.com/t5/NFC/NTAG-216-ISO-14443-part-4/m-p/777301#M3761</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Dear Sir,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;I have some question for the chip Ntag 216. This is because I did not locate the answer on the spec sheet as attached.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;1) &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;“The Reading of this Chip Cards uses commands which are in the specifications ISO 7816 und EMV defined, For sending the commands is Norm ISO-14443, inclusive part 4 necessary.” &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Any supporting for the chip Inputting and Outputting. What is the Transmission protocol?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;What is the different from ISO 7816 and&amp;nbsp; ISO 14443 ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;3)&amp;nbsp;&lt;SPAN&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;Our terminal currently only supports smart card commands over the NFC interface, which is sometimes called “chip emulation mode” or “ISO-14443 part 4 support”. Can you please tell me, if your NFC chip supports this mode?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;SPAN&gt;Thank you&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;SPAN&gt;Samuel Po&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Feb 2018 09:06:10 GMT</pubDate>
    <dc:creator>posamuel</dc:creator>
    <dc:date>2018-02-27T09:06:10Z</dc:date>
    <item>
      <title>NTAG 216 - ISO 14443 - part 4</title>
      <link>https://community.nxp.com/t5/NFC/NTAG-216-ISO-14443-part-4/m-p/777301#M3761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Dear Sir,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;I have some question for the chip Ntag 216. This is because I did not locate the answer on the spec sheet as attached.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;1) &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;“The Reading of this Chip Cards uses commands which are in the specifications ISO 7816 und EMV defined, For sending the commands is Norm ISO-14443, inclusive part 4 necessary.” &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Any supporting for the chip Inputting and Outputting. What is the Transmission protocol?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;What is the different from ISO 7816 and&amp;nbsp; ISO 14443 ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;3)&amp;nbsp;&lt;SPAN&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;Our terminal currently only supports smart card commands over the NFC interface, which is sometimes called “chip emulation mode” or “ISO-14443 part 4 support”. Can you please tell me, if your NFC chip supports this mode?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;SPAN&gt;Thank you&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;SPAN&gt;Samuel Po&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Feb 2018 09:06:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG-216-ISO-14443-part-4/m-p/777301#M3761</guid>
      <dc:creator>posamuel</dc:creator>
      <dc:date>2018-02-27T09:06:10Z</dc:date>
    </item>
    <item>
      <title>Re: NTAG 216 - ISO 14443 - part 4</title>
      <link>https://community.nxp.com/t5/NFC/NTAG-216-ISO-14443-part-4/m-p/777302#M3762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="314161" data-username="posamuel" href="https://community.nxp.com/people/posamuel"&gt;PO Samuel&lt;/A&gt;, sorry for the delay,&amp;nbsp; to answer your questions;&amp;nbsp;the NTAG 216 is a type 2 tags this means it does not support the same command set as the smart cards, this tags supports&amp;nbsp; ISO&amp;nbsp;14443-3&amp;nbsp; not the part 4 this is more from the MIFARE family, the only NTAG that&amp;nbsp;&amp;nbsp;is also compliant to ISO/IEC14443-4, ISO/IEC 7816-4 file structure and APDUs formats the NTAG 413 DNA,&amp;nbsp; the ISO 14443 is a norm for contactless,&amp;nbsp; the ISO 7816 it is divided in 4 parts the first 3 parts are for contact communication and describe the physical layer and the part 4 is the standardization of the command set&amp;nbsp; that is why some of our tags comply with 7816 but it is specified that only the part 4.&amp;nbsp; &amp;nbsp;this tag does not support the ISO 14443-4.&amp;nbsp;&lt;/P&gt;&lt;P&gt;hope this was clear enough if not please let me know.&lt;/P&gt;&lt;P&gt;Have a great day !&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Mar 2018 19:29:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG-216-ISO-14443-part-4/m-p/777302#M3762</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2018-03-27T19:29:12Z</dc:date>
    </item>
  </channel>
</rss>