<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックNT3H2111  SRAM Mirror</title>
    <link>https://community.nxp.com/t5/NFC/NT3H2111-SRAM-Mirror/m-p/769844#M3618</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd like to write some data from my micro (I2C side) to the SRAM of a NT3H2111. I also want to be able to modify the SRAM via an app on my phone, so I decided to enable the SRAM mirror (SRAM_MIRROR_ON_OFF = 1) and to disable the pass-through (PTHROU_ON_OFF = 0).&lt;/P&gt;&lt;P&gt;I have also chosen 0x01 as SRAM_MIRROR_BLOCK.&lt;/P&gt;&lt;P&gt;My questions are :&lt;/P&gt;&lt;P&gt;1) Is the eeprom endurance go down each time I write on SRAM via I2C ?&lt;/P&gt;&lt;P&gt;2) Is the eeprom endurance go down each time I write on SRAM via the NFC ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Riccardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Jun 2018 12:57:13 GMT</pubDate>
    <dc:creator>straga_riccardo</dc:creator>
    <dc:date>2018-06-11T12:57:13Z</dc:date>
    <item>
      <title>NT3H2111  SRAM Mirror</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-SRAM-Mirror/m-p/769844#M3618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd like to write some data from my micro (I2C side) to the SRAM of a NT3H2111. I also want to be able to modify the SRAM via an app on my phone, so I decided to enable the SRAM mirror (SRAM_MIRROR_ON_OFF = 1) and to disable the pass-through (PTHROU_ON_OFF = 0).&lt;/P&gt;&lt;P&gt;I have also chosen 0x01 as SRAM_MIRROR_BLOCK.&lt;/P&gt;&lt;P&gt;My questions are :&lt;/P&gt;&lt;P&gt;1) Is the eeprom endurance go down each time I write on SRAM via I2C ?&lt;/P&gt;&lt;P&gt;2) Is the eeprom endurance go down each time I write on SRAM via the NFC ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Riccardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jun 2018 12:57:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-SRAM-Mirror/m-p/769844#M3618</guid>
      <dc:creator>straga_riccardo</dc:creator>
      <dc:date>2018-06-11T12:57:13Z</dc:date>
    </item>
    <item>
      <title>Re: NT3H2111  SRAM Mirror</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-SRAM-Mirror/m-p/769845#M3619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, the fact that the SRAM is mirrored to the EEPROM means that the SRAM will be accessible to the NFC interface. This way, you will be writing to / reading from the SRAM directly on both interfaces.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more information, please refer to chapter 8.3.4 of the data-sheet:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/data-sheet/NT3H2111_2211.pdf" title="https://www.nxp.com/docs/en/data-sheet/NT3H2111_2211.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/NT3H2111_2211.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jun 2018 22:46:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-SRAM-Mirror/m-p/769845#M3619</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2018-06-15T22:46:40Z</dc:date>
    </item>
  </channel>
</rss>