<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Authenticate desfire ev1 in android phone in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Authenticate-desfire-ev1-in-android-phone/m-p/761386#M3483</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I have a PAX device with a sam card and a desfire ev1 card.&lt;/P&gt;&lt;P&gt;I use a application that use PAX library to debit from this card.&lt;/P&gt;&lt;P&gt;It works fine when I use PAX device.&lt;/P&gt;&lt;P&gt;I want to do the same as above but by use an android phone device that have nfc reader.&lt;/P&gt;&lt;P&gt;The scenario is, I communicate by desfire card with android library(android.nfc.tech.IsoDep) in phone device and I communicate by sam card in PAX device and connect to device by a socket in network.&lt;/P&gt;&lt;P&gt;I get card UID and select application in phone device successfully.&lt;/P&gt;&lt;P&gt;In next step(Authenticate Key 1) I send require data to PAX device.&lt;/P&gt;&lt;P&gt;In PAX device give receive data to sam and get data from sam reader then Send them to phone device.&lt;/P&gt;&lt;P&gt;In phone device give receive data to card. but in this step card return this error : 91, 1c&lt;/P&gt;&lt;P&gt;I have these questions :&lt;/P&gt;&lt;P&gt;Is this possible in logically?&lt;/P&gt;&lt;P&gt;If it is possible can help me?&lt;/P&gt;&lt;P&gt;What is wrong in this solution?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 28 Jan 2018 12:08:56 GMT</pubDate>
    <dc:creator>jackjohnson2018</dc:creator>
    <dc:date>2018-01-28T12:08:56Z</dc:date>
    <item>
      <title>Authenticate desfire ev1 in android phone</title>
      <link>https://community.nxp.com/t5/NFC/Authenticate-desfire-ev1-in-android-phone/m-p/761386#M3483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I have a PAX device with a sam card and a desfire ev1 card.&lt;/P&gt;&lt;P&gt;I use a application that use PAX library to debit from this card.&lt;/P&gt;&lt;P&gt;It works fine when I use PAX device.&lt;/P&gt;&lt;P&gt;I want to do the same as above but by use an android phone device that have nfc reader.&lt;/P&gt;&lt;P&gt;The scenario is, I communicate by desfire card with android library(android.nfc.tech.IsoDep) in phone device and I communicate by sam card in PAX device and connect to device by a socket in network.&lt;/P&gt;&lt;P&gt;I get card UID and select application in phone device successfully.&lt;/P&gt;&lt;P&gt;In next step(Authenticate Key 1) I send require data to PAX device.&lt;/P&gt;&lt;P&gt;In PAX device give receive data to sam and get data from sam reader then Send them to phone device.&lt;/P&gt;&lt;P&gt;In phone device give receive data to card. but in this step card return this error : 91, 1c&lt;/P&gt;&lt;P&gt;I have these questions :&lt;/P&gt;&lt;P&gt;Is this possible in logically?&lt;/P&gt;&lt;P&gt;If it is possible can help me?&lt;/P&gt;&lt;P&gt;What is wrong in this solution?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Jan 2018 12:08:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Authenticate-desfire-ev1-in-android-phone/m-p/761386#M3483</guid>
      <dc:creator>jackjohnson2018</dc:creator>
      <dc:date>2018-01-28T12:08:56Z</dc:date>
    </item>
    <item>
      <title>Re: Authenticate desfire ev1 in android phone</title>
      <link>https://community.nxp.com/t5/NFC/Authenticate-desfire-ev1-in-android-phone/m-p/761387#M3484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jack,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the key type used in your test?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Feb 2018 08:37:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Authenticate-desfire-ev1-in-android-phone/m-p/761387#M3484</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2018-02-01T08:37:02Z</dc:date>
    </item>
  </channel>
</rss>