<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 How can I upload a chip coding into the NFC chips (NHS3152 or NHS3152 UK) without PCB-LPC-Link2?</title>
    <link>https://community.nxp.com/t5/NFC/How-can-I-upload-a-chip-coding-into-the-NFC-chips-NHS3152-or/m-p/756434#M3395</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I bought NFC chips (NHS3152 and NHS3152UK) for the demonstration of IoT. For the demo PCB based on NHS 3152 (such as, NHS3152 General Starter Kit), the chip coding can be uploaded using LPC-Link2.&lt;/P&gt;&lt;P&gt;But, I need to use the NFC chips, not demo PCBs. If so how can I upload a chip coding to the NFC chips (NHS3152 or NHS3152 UK) without PCB-LPC-Link2?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Apr 2018 12:33:28 GMT</pubDate>
    <dc:creator>jihunpark</dc:creator>
    <dc:date>2018-04-23T12:33:28Z</dc:date>
    <item>
      <title>How can I upload a chip coding into the NFC chips (NHS3152 or NHS3152 UK) without PCB-LPC-Link2?</title>
      <link>https://community.nxp.com/t5/NFC/How-can-I-upload-a-chip-coding-into-the-NFC-chips-NHS3152-or/m-p/756434#M3395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I bought NFC chips (NHS3152 and NHS3152UK) for the demonstration of IoT. For the demo PCB based on NHS 3152 (such as, NHS3152 General Starter Kit), the chip coding can be uploaded using LPC-Link2.&lt;/P&gt;&lt;P&gt;But, I need to use the NFC chips, not demo PCBs. If so how can I upload a chip coding to the NFC chips (NHS3152 or NHS3152 UK) without PCB-LPC-Link2?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Apr 2018 12:33:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/How-can-I-upload-a-chip-coding-into-the-NFC-chips-NHS3152-or/m-p/756434#M3395</guid>
      <dc:creator>jihunpark</dc:creator>
      <dc:date>2018-04-23T12:33:28Z</dc:date>
    </item>
    <item>
      <title>Re: How can I upload a chip coding into the NFC chips (NHS3152 or NHS3152 UK) without PCB-LPC-Link2?</title>
      <link>https://community.nxp.com/t5/NFC/How-can-I-upload-a-chip-coding-into-the-NFC-chips-NHS3152-or/m-p/756435#M3396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please have a look &lt;EM&gt;AN_NHS31xx_Flashing.pdf&lt;/EM&gt;, available in the SDK under the docs folder. It describes the different ways to load firmware into the chip. Any wired approach will make use of the LPC-Link2 board, but we also provide a &lt;SPAN style="text-decoration: underline;"&gt;one-time&lt;/SPAN&gt; wireless download using the NFC interface and an Android APP or a PC-based Python script.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best,&lt;BR /&gt;Dries.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Apr 2018 06:47:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/How-can-I-upload-a-chip-coding-into-the-NFC-chips-NHS3152-or/m-p/756435#M3396</guid>
      <dc:creator>driesmoors</dc:creator>
      <dc:date>2018-04-27T06:47:06Z</dc:date>
    </item>
  </channel>
</rss>