<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Tagwriter problem on windows 10 in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Tagwriter-problem-on-windows-10/m-p/754079#M3335</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having trouble getting tagwriter to work on a Dell Inspiron 5000 laptop running Windows 10 using an external Sony S380 tag reader.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I installed the Sony drivers, and the Sony NFC Port/PaSoRi diagnostic tool says it is working ok.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, the windows 10 tagwriter app reports “Read from NFC object!” – “No Proximity device detected”.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there some further configuration needed to make tagwriter work on windows 10?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 22 Apr 2018 10:24:32 GMT</pubDate>
    <dc:creator>ianbowditch</dc:creator>
    <dc:date>2018-04-22T10:24:32Z</dc:date>
    <item>
      <title>Tagwriter problem on windows 10</title>
      <link>https://community.nxp.com/t5/NFC/Tagwriter-problem-on-windows-10/m-p/754079#M3335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having trouble getting tagwriter to work on a Dell Inspiron 5000 laptop running Windows 10 using an external Sony S380 tag reader.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I installed the Sony drivers, and the Sony NFC Port/PaSoRi diagnostic tool says it is working ok.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, the windows 10 tagwriter app reports “Read from NFC object!” – “No Proximity device detected”.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there some further configuration needed to make tagwriter work on windows 10?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 22 Apr 2018 10:24:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Tagwriter-problem-on-windows-10/m-p/754079#M3335</guid>
      <dc:creator>ianbowditch</dc:creator>
      <dc:date>2018-04-22T10:24:32Z</dc:date>
    </item>
  </channel>
</rss>