<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックNTAG213 Dynamic Lock Bytes</title>
    <link>https://community.nxp.com/t5/NFC/NTAG213-Dynamic-Lock-Bytes/m-p/518609#M325</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am reading/writing an RFID tag that uses an NTAG213 IC and the Dynamic Lock Bytes are not working as I expected.&amp;nbsp; I have written bytes 0, 1 and 2 of the dynamic lock bytes to the values 0x00, 0x00, 0x3f respectively with the assumption that would render pages 16 through 19 of the memory as read-only.&amp;nbsp; However, I just discovered that I am able to write and modify the memory in at least pages 16 and 17 (I have not tried writing to any of the other pages that I thought were locked).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there more to these lock bytes than simply setting the bits that correspond to the pages for which read-only access is desired?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any information would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Jun 2016 21:46:11 GMT</pubDate>
    <dc:creator>ArtyCF</dc:creator>
    <dc:date>2016-06-10T21:46:11Z</dc:date>
    <item>
      <title>NTAG213 Dynamic Lock Bytes</title>
      <link>https://community.nxp.com/t5/NFC/NTAG213-Dynamic-Lock-Bytes/m-p/518609#M325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am reading/writing an RFID tag that uses an NTAG213 IC and the Dynamic Lock Bytes are not working as I expected.&amp;nbsp; I have written bytes 0, 1 and 2 of the dynamic lock bytes to the values 0x00, 0x00, 0x3f respectively with the assumption that would render pages 16 through 19 of the memory as read-only.&amp;nbsp; However, I just discovered that I am able to write and modify the memory in at least pages 16 and 17 (I have not tried writing to any of the other pages that I thought were locked).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there more to these lock bytes than simply setting the bits that correspond to the pages for which read-only access is desired?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any information would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jun 2016 21:46:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG213-Dynamic-Lock-Bytes/m-p/518609#M325</guid>
      <dc:creator>ArtyCF</dc:creator>
      <dc:date>2016-06-10T21:46:11Z</dc:date>
    </item>
    <item>
      <title>Re: NTAG213 Dynamic Lock Bytes</title>
      <link>https://community.nxp.com/t5/NFC/NTAG213-Dynamic-Lock-Bytes/m-p/518610#M326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Steve:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for using the NFC community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that you did not use the LOCK bytes of NTAG213 in the correct order and writing a wrong value. You said you wanted to lock pages 16 to 19 using dynamic lock bytes [0x00 0x00 0x3F]. The actual values to lock pages 16/17/18/19 should be [0x03 0x00 0x00]. See the picture below from NTAG213 datasheet:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59772i22F57D3DD4B9FAFA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the values you used you are actually enabling the &lt;STRONG&gt;Block Locking&lt;/STRONG&gt; bits (&lt;STRONG&gt;BL&lt;/STRONG&gt;). With those bits set to 1, the corresponding page locking bits cannot be written anymore.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this clarifies. Let me know if you have questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 02:25:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG213-Dynamic-Lock-Bytes/m-p/518610#M326</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2016-06-17T02:25:44Z</dc:date>
    </item>
  </channel>
</rss>