<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic switching security level SL1 to SL3 in NFC</title>
    <link>https://community.nxp.com/t5/NFC/switching-security-level-SL1-to-SL3/m-p/744184#M3192</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using NXP om5577 device on raspbery pi board (win10 iot), mifire plus se card, C#.&lt;/P&gt;&lt;P&gt;I am stuck with switching&amp;nbsp; security level SL1 -&amp;gt; SL3. Sending apdu command FF C2 00 02 04 8F 02 00 04 (set to ISO 14443-4 Type A, communication layer 4) returns 6F00 - internal exception. On ACS ACR1281 1S Dual Reader PICC 0 this cmd works fine.&lt;/P&gt;&lt;P&gt;What could be wrong?&lt;/P&gt;&lt;P&gt;Switching from SL0 to SL1 works fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Apr 2018 11:00:00 GMT</pubDate>
    <dc:creator>ragazor</dc:creator>
    <dc:date>2018-04-18T11:00:00Z</dc:date>
    <item>
      <title>switching security level SL1 to SL3</title>
      <link>https://community.nxp.com/t5/NFC/switching-security-level-SL1-to-SL3/m-p/744184#M3192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using NXP om5577 device on raspbery pi board (win10 iot), mifire plus se card, C#.&lt;/P&gt;&lt;P&gt;I am stuck with switching&amp;nbsp; security level SL1 -&amp;gt; SL3. Sending apdu command FF C2 00 02 04 8F 02 00 04 (set to ISO 14443-4 Type A, communication layer 4) returns 6F00 - internal exception. On ACS ACR1281 1S Dual Reader PICC 0 this cmd works fine.&lt;/P&gt;&lt;P&gt;What could be wrong?&lt;/P&gt;&lt;P&gt;Switching from SL0 to SL1 works fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Apr 2018 11:00:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/switching-security-level-SL1-to-SL3/m-p/744184#M3192</guid>
      <dc:creator>ragazor</dc:creator>
      <dc:date>2018-04-18T11:00:00Z</dc:date>
    </item>
    <item>
      <title>Re: switching security level SL1 to SL3</title>
      <link>https://community.nxp.com/t5/NFC/switching-security-level-SL1-to-SL3/m-p/744185#M3193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="317381" data-username="ragazor" href="https://community.nxp.com/people/ragazor"&gt;Yurii Oliinyk&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;In the state SL1 MF Classic Authenticated, the MF1SEP(H)10x1 will behave as&lt;BR /&gt;MIFARE Classic 1K with the possibility of optional AES authentication.&lt;BR /&gt;A full card activation to ISO 14443-4 is needed to Authenticate with the Originality Key or&amp;nbsp; Authenticate with the SL3 Switch Key. The authentication can be done both as&lt;BR /&gt;First Authentication, described in Section 7.6.2.1 or as Following Authentication,&lt;BR /&gt;described in Section 7.6.2.2. Respective Keys as described in Section 8.6 have to&lt;BR /&gt;be used. After authentication with SL3 Switch Key a reset and card activation are&lt;BR /&gt;needed to start operating in the security level 3.&lt;/P&gt;&lt;P&gt;please check the full data sheet in the section 7.5 in order to see how the level switching can be performed.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jun 2018 16:41:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/switching-security-level-SL1-to-SL3/m-p/744185#M3193</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2018-06-01T16:41:33Z</dc:date>
    </item>
  </channel>
</rss>