<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CLEV6630B not recognized by usb  in NFC</title>
    <link>https://community.nxp.com/t5/NFC/CLEV6630B-not-recognized-by-usb/m-p/735712#M3093</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a CLEV6630B and it seems to be in a stuck or looped state, it will not connect or is recognized by my computers USB port any longer. Is there something I can try?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 May 2018 12:34:11 GMT</pubDate>
    <dc:creator>wegelinj</dc:creator>
    <dc:date>2018-05-30T12:34:11Z</dc:date>
    <item>
      <title>CLEV6630B not recognized by usb</title>
      <link>https://community.nxp.com/t5/NFC/CLEV6630B-not-recognized-by-usb/m-p/735712#M3093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a CLEV6630B and it seems to be in a stuck or looped state, it will not connect or is recognized by my computers USB port any longer. Is there something I can try?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2018 12:34:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLEV6630B-not-recognized-by-usb/m-p/735712#M3093</guid>
      <dc:creator>wegelinj</dc:creator>
      <dc:date>2018-05-30T12:34:11Z</dc:date>
    </item>
    <item>
      <title>Re: CLEV6630B not recognized by usb</title>
      <link>https://community.nxp.com/t5/NFC/CLEV6630B-not-recognized-by-usb/m-p/735713#M3094</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jackson,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you program the board with correct firmware? If you use cockpit with it , you may find the firmware in the installation folder as below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18919i9C8792E17925A6A8/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;To download the firmware, please refer to &lt;A href="https://community.nxp.com/docs/DOC-334997"&gt;Program the firmware to PNEV5180B board&lt;/A&gt; for details.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 06:42:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLEV6630B-not-recognized-by-usb/m-p/735713#M3094</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2018-06-06T06:42:34Z</dc:date>
    </item>
  </channel>
</rss>