<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Security system using MFRC522 and Micro controller (NXP or Atmel)  in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Security-system-using-MFRC522-and-Micro-controller-NXP-or-Atmel/m-p/731813#M3036</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am working on a security system and I am planning to use RFID chip MFRC522 and the micro-controller that will manage the communication with the RFID will be pic18F452, is this a right combination from the point of view of security?&lt;/P&gt;&lt;P&gt;Also, my friends told me that I should use chips from Atmel like "ATmega1284P" because of security issues and the &lt;SPAN&gt;pic18F452 could be hacked&lt;/SPAN&gt;, is this right? and would you please recommend micro-controller for my case.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Nov 2017 07:53:59 GMT</pubDate>
    <dc:creator>moustafaeldysou</dc:creator>
    <dc:date>2017-11-23T07:53:59Z</dc:date>
    <item>
      <title>Security system using MFRC522 and Micro controller (NXP or Atmel)</title>
      <link>https://community.nxp.com/t5/NFC/Security-system-using-MFRC522-and-Micro-controller-NXP-or-Atmel/m-p/731813#M3036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am working on a security system and I am planning to use RFID chip MFRC522 and the micro-controller that will manage the communication with the RFID will be pic18F452, is this a right combination from the point of view of security?&lt;/P&gt;&lt;P&gt;Also, my friends told me that I should use chips from Atmel like "ATmega1284P" because of security issues and the &lt;SPAN&gt;pic18F452 could be hacked&lt;/SPAN&gt;, is this right? and would you please recommend micro-controller for my case.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Nov 2017 07:53:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Security-system-using-MFRC522-and-Micro-controller-NXP-or-Atmel/m-p/731813#M3036</guid>
      <dc:creator>moustafaeldysou</dc:creator>
      <dc:date>2017-11-23T07:53:59Z</dc:date>
    </item>
    <item>
      <title>Re: Security system using MFRC522 and Micro controller (NXP or Atmel)</title>
      <link>https://community.nxp.com/t5/NFC/Security-system-using-MFRC522-and-Micro-controller-NXP-or-Atmel/m-p/731814#M3037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As mentioned in the internal case:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently, the PNEV512B implements an LPC1769 for&amp;nbsp;&lt;BR /&gt;controlling the NFC Front End.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fproducts%2Fidentification-and-security%2Fnfc%2Fnfc-reader-ics%2Fpn512-reader-board%3APNEV512B%3Flang_cd%3Den" rel="nofollow" target="_blank"&gt;https://www.nxp.com/products/identification-and-security/nfc/nfc-reader-ics/pn512-reader-board:PNEV512B?lang_cd=en&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;PNEV512B is the evaluation board compatible with MFRC522&amp;nbsp;&lt;BR /&gt;Front End for which the NFC Reader Library is compatible as well. This way you&amp;nbsp;&lt;BR /&gt;can interface LPC1769 to MFRC522 through SPI, UART or I2C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Otherwise, if you need a securer host MCU you can refer to LPC18Sxx&amp;nbsp;&lt;BR /&gt;Family with security features for protecting code and data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Ffact-sheet%2FLPC18SXXLF.pdf%3Ffsrch%3D1%26sr%3D4%26pageNum%3D1" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/fact-sheet/LPC18SXXLF.pdf?fsrch=1&amp;amp;sr=4&amp;amp;pageNum=1&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Dec 2017 22:46:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Security-system-using-MFRC522-and-Micro-controller-NXP-or-Atmel/m-p/731814#M3037</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2017-12-04T22:46:30Z</dc:date>
    </item>
  </channel>
</rss>