<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic P2P exchange + Powerdown timing problem in NFC</title>
    <link>https://community.nxp.com/t5/NFC/P2P-exchange-Powerdown-timing-problem/m-p/727593#M2979</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I bougth two PN532. I implement P2P communication with DEP protocol in active mode. After communication, both PN532 receives the command "POWERDOWN 0x88 0x01"&amp;nbsp; (=Wake up on RF field &amp;amp; I2C and Generate an IRQ on wake up). Answer is correct and there is no error code. PROBLEM : when the target powers down before the initiator does, the "wake up on rf field" does not work anymore.What can I do?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 06 May 2018 05:45:46 GMT</pubDate>
    <dc:creator>romane</dc:creator>
    <dc:date>2018-05-06T05:45:46Z</dc:date>
    <item>
      <title>P2P exchange + Powerdown timing problem</title>
      <link>https://community.nxp.com/t5/NFC/P2P-exchange-Powerdown-timing-problem/m-p/727593#M2979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I bougth two PN532. I implement P2P communication with DEP protocol in active mode. After communication, both PN532 receives the command "POWERDOWN 0x88 0x01"&amp;nbsp; (=Wake up on RF field &amp;amp; I2C and Generate an IRQ on wake up). Answer is correct and there is no error code. PROBLEM : when the target powers down before the initiator does, the "wake up on rf field" does not work anymore.What can I do?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 May 2018 05:45:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/P2P-exchange-Powerdown-timing-problem/m-p/727593#M2979</guid>
      <dc:creator>romane</dc:creator>
      <dc:date>2018-05-06T05:45:46Z</dc:date>
    </item>
    <item>
      <title>Re: P2P exchange + Powerdown timing problem</title>
      <link>https://community.nxp.com/t5/NFC/P2P-exchange-Powerdown-timing-problem/m-p/727594#M2980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please make sure that CIU_wu_en is enabled as a wake-up source. For more information please refer to Table 144 of the data-sheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The sensitivity of the RF level detector is adjustable in a 4-bit range, please refer to chapter 8.6.8 RF level detector of the data-sheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As well, verify if RF level detector is enabled as mentioned in chapter 8.5.4 Soft-Power-Down mode (SPD) of the data-sheet:&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/nxp/data-sheets/PN532_C1.pdf" title="https://www.nxp.com/docs/en/nxp/data-sheets/PN532_C1.pdf"&gt;https://www.nxp.com/docs/en/nxp/data-sheets/PN532_C1.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jun 2018 16:12:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/P2P-exchange-Powerdown-timing-problem/m-p/727594#M2980</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2018-06-29T16:12:42Z</dc:date>
    </item>
  </channel>
</rss>