<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックPN7462 Eval GPIO use and running without debugger</title>
    <link>https://community.nxp.com/t5/NFC/PN7462-Eval-GPIO-use-and-running-without-debugger/m-p/726994#M2972</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to trigger GPIO outputs with a card read. Seems simple enough, but only some of the outputs are working, Other outputs put out a very short pulse when the bit is set on.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking at the full board schematic (which for some reason is not included in the kit) it seems some GPIO pins are shared with the debugger. GPIO 5,6,7,8. &amp;nbsp;Am I correct in that if you are using the debugger, you cannot use these pins as GPIO? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I wanted to run the eval board stand alone, how would I do that? &amp;nbsp;If I boot it without the debugger connected, nothing happens.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will need the HSU next. Are those pins also used with the debugger? Or will I be able to use them while the debugger is connected?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 16 Dec 2017 20:04:58 GMT</pubDate>
    <dc:creator>turbo2ltr</dc:creator>
    <dc:date>2017-12-16T20:04:58Z</dc:date>
    <item>
      <title>PN7462 Eval GPIO use and running without debugger</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Eval-GPIO-use-and-running-without-debugger/m-p/726994#M2972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to trigger GPIO outputs with a card read. Seems simple enough, but only some of the outputs are working, Other outputs put out a very short pulse when the bit is set on.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking at the full board schematic (which for some reason is not included in the kit) it seems some GPIO pins are shared with the debugger. GPIO 5,6,7,8. &amp;nbsp;Am I correct in that if you are using the debugger, you cannot use these pins as GPIO? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I wanted to run the eval board stand alone, how would I do that? &amp;nbsp;If I boot it without the debugger connected, nothing happens.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will need the HSU next. Are those pins also used with the debugger? Or will I be able to use them while the debugger is connected?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Dec 2017 20:04:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Eval-GPIO-use-and-running-without-debugger/m-p/726994#M2972</guid>
      <dc:creator>turbo2ltr</dc:creator>
      <dc:date>2017-12-16T20:04:58Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 Eval GPIO use and running without debugger</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Eval-GPIO-use-and-running-without-debugger/m-p/726995#M2973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mike,&lt;/P&gt;&lt;P&gt;(1) Configure them to be GPIO: No problem.&lt;/P&gt;&lt;P&gt;See UM10858.pdf : &lt;A href="https://www.nxp.com/docs/en/user-guide/UM10858.pdf"&gt;https://www.nxp.com/docs/en/user-guide/UM10858.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31805iE91B568C22E70342/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31759i2C68816EE85F60B5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31838iA698A52972D27BD3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;(2) Debugger will use SWD interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;TIC weidong sun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Dec 2017 07:59:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Eval-GPIO-use-and-running-without-debugger/m-p/726995#M2973</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2017-12-21T07:59:56Z</dc:date>
    </item>
  </channel>
</rss>