<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックMCU Express IDE doesn't recognise CMSIS - DAP debug probe LPC Link2.</title>
    <link>https://community.nxp.com/t5/NFC/MCU-Express-IDE-doesn-t-recognise-CMSIS-DAP-debug-probe-LPC/m-p/716917#M2812</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to run #PN7462 Examples using the OM27462 Development Kit on #MCU Express IDE. For debugging I use LPC Link2 debug probe. I also use #LPC Scrypt to update the firmware of debug probe. However, just for the first time, the IDE detects CMSIS - DAP debug probe, it doesn't recognize the probe after first time. I tried debugging the &lt;STRONG&gt;PN27462U_ex_phExMain &lt;/STRONG&gt;example, but LEDs are not glowing or the board is not going in the polling mode. I also tried running other examples, and I am facing the same issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;May i know the right way to use the debug probe. I also tried flashing the binary file on the board in SWD mode, still the code is not running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Abhijit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Apr 2018 23:30:12 GMT</pubDate>
    <dc:creator>abhijitkatkar</dc:creator>
    <dc:date>2018-04-09T23:30:12Z</dc:date>
    <item>
      <title>MCU Express IDE doesn't recognise CMSIS - DAP debug probe LPC Link2.</title>
      <link>https://community.nxp.com/t5/NFC/MCU-Express-IDE-doesn-t-recognise-CMSIS-DAP-debug-probe-LPC/m-p/716917#M2812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to run #PN7462 Examples using the OM27462 Development Kit on #MCU Express IDE. For debugging I use LPC Link2 debug probe. I also use #LPC Scrypt to update the firmware of debug probe. However, just for the first time, the IDE detects CMSIS - DAP debug probe, it doesn't recognize the probe after first time. I tried debugging the &lt;STRONG&gt;PN27462U_ex_phExMain &lt;/STRONG&gt;example, but LEDs are not glowing or the board is not going in the polling mode. I also tried running other examples, and I am facing the same issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;May i know the right way to use the debug probe. I also tried flashing the binary file on the board in SWD mode, still the code is not running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Abhijit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Apr 2018 23:30:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MCU-Express-IDE-doesn-t-recognise-CMSIS-DAP-debug-probe-LPC/m-p/716917#M2812</guid>
      <dc:creator>abhijitkatkar</dc:creator>
      <dc:date>2018-04-09T23:30:12Z</dc:date>
    </item>
    <item>
      <title>Re: MCU Express IDE doesn't recognise CMSIS - DAP debug probe LPC Link2.</title>
      <link>https://community.nxp.com/t5/NFC/MCU-Express-IDE-doesn-t-recognise-CMSIS-DAP-debug-probe-LPC/m-p/716918#M2813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Abhijit，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For CMSIS-DAP, the Windows driver package if not already installed – for example by LPCXpresso IDE – can be found at:&lt;BR /&gt;&lt;A href="http://www.lpcware.com/content/nxpfile/lpcxpresso-link2-usb-driverpackage"&gt;http://www.lpcware.com/content/nxpfile/lpcxpresso-link2-usb-driverpackage&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In addition, there is a small possibility that an incompatible driver may be selected. For more details of this issue and fix, please see the FAQ below:&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/630660"&gt;https://community.nxp.com/message/630660&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may also update its firmware to act as a j-link debug probe and check if it works on your side. Please refer to &lt;A class="jivelink10" href="https://www.nxp.com/docs/en/supporting-information/Debug_Probe_Firmware_Programming.pdf" title="https://www.nxp.com/docs/en/supporting-information/Debug_Probe_Firmware_Programming.pdf"&gt;https://www.nxp.com/docs/en/supporting-information/Debug_Probe_Firmware_Programming.pdf&lt;/A&gt; for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Apr 2018 11:47:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MCU-Express-IDE-doesn-t-recognise-CMSIS-DAP-debug-probe-LPC/m-p/716918#M2813</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2018-04-16T11:47:13Z</dc:date>
    </item>
  </channel>
</rss>