<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックBuilding explore-nfc from source on Pi</title>
    <link>https://community.nxp.com/t5/NFC/Building-explore-nfc-from-source-on-Pi/m-p/706029#M2642</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can anyone outline the correct way to build the NFC Explorer software stack for Raspbian Jessie?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The documentation in AN11802.pdf does not result in a clean compile.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Two artifacts are available: SW3693.zip and SW282816.zip&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board I am using this with is NXP-EXPLORER 1.6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking through the source code from SW3693.zip, I am not finding support for this board. I could be wrong, of course, but if I am right, I am wondering if the SW3693.zip version is incorrect for support for that board.&lt;/P&gt;&lt;P&gt;If it is incorrect, is there a link available to the correct version of SW3693.zip that does support the board?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Aug 2017 15:10:10 GMT</pubDate>
    <dc:creator>noelkendall</dc:creator>
    <dc:date>2017-08-24T15:10:10Z</dc:date>
    <item>
      <title>Building explore-nfc from source on Pi</title>
      <link>https://community.nxp.com/t5/NFC/Building-explore-nfc-from-source-on-Pi/m-p/706029#M2642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can anyone outline the correct way to build the NFC Explorer software stack for Raspbian Jessie?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The documentation in AN11802.pdf does not result in a clean compile.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Two artifacts are available: SW3693.zip and SW282816.zip&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board I am using this with is NXP-EXPLORER 1.6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking through the source code from SW3693.zip, I am not finding support for this board. I could be wrong, of course, but if I am right, I am wondering if the SW3693.zip version is incorrect for support for that board.&lt;/P&gt;&lt;P&gt;If it is incorrect, is there a link available to the correct version of SW3693.zip that does support the board?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Aug 2017 15:10:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Building-explore-nfc-from-source-on-Pi/m-p/706029#M2642</guid>
      <dc:creator>noelkendall</dc:creator>
      <dc:date>2017-08-24T15:10:10Z</dc:date>
    </item>
  </channel>
</rss>