<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Need help with PN7462 configuration in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Need-help-with-PN7462-configuration/m-p/692637#M2469</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;:smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Aug 2018 07:36:15 GMT</pubDate>
    <dc:creator>276642088</dc:creator>
    <dc:date>2018-08-10T07:36:15Z</dc:date>
    <item>
      <title>Need help with PN7462 configuration</title>
      <link>https://community.nxp.com/t5/NFC/Need-help-with-PN7462-configuration/m-p/692634#M2466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello guys, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my current project, I'm using PN7462 module from NXP. I need that module for the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. To communicate with NFC card&lt;/P&gt;&lt;P&gt;2. To communicate with GSM module via UART interface.&amp;nbsp;I need to have 1.8V level UART communication with GSM unit. Configuration commands for GSM should be sent from PN7462 to GSM.&amp;nbsp;&lt;/P&gt;&lt;P&gt;3. To control a few of the GPIO signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm reading PN7462 datasheet but I'm not sure I can digest it in a way to properly design my board. Would you guys be so kind to help me with the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. How to supply the PN7462 module? Which power pins do I need to connect to power supply? How to achieve 1.8V for UART and GPIOs?&lt;/P&gt;&lt;P&gt;2. How to download the firmware on PN7462? Using SWD interface ?&lt;/P&gt;&lt;P&gt;3. How to properly design the antenna circuit for NFC communication. Is there any antenna chip available on the market or I need to print it on a PCB?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your time and effort. Really appreciate it.&lt;/P&gt;&lt;P&gt;Looking forward to reading from you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;P&gt;Bojan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2017 13:05:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Need-help-with-PN7462-configuration/m-p/692634#M2466</guid>
      <dc:creator>bojanjovanovic</dc:creator>
      <dc:date>2017-06-20T13:05:27Z</dc:date>
    </item>
    <item>
      <title>Re: Need help with PN7462 configuration</title>
      <link>https://community.nxp.com/t5/NFC/Need-help-with-PN7462-configuration/m-p/692635#M2467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By reading a PN7462 datasheet, I noticed that it has a high-speed UART which can operate in slave mode only. What actually does that means?&lt;/P&gt;&lt;P&gt;Will I be able to control GSM module through that HSUART in a way to send AT commands from PN7462 and to read the response of GSM module?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bojan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jun 2017 07:47:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Need-help-with-PN7462-configuration/m-p/692635#M2467</guid>
      <dc:creator>bojanjovanovic</dc:creator>
      <dc:date>2017-06-21T07:47:42Z</dc:date>
    </item>
    <item>
      <title>Re: Need help with PN7462 configuration</title>
      <link>https://community.nxp.com/t5/NFC/Need-help-with-PN7462-configuration/m-p/692636#M2468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bojan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please kindly refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. How to supply the PN7462 module? Which power pins do I need to connect to power supply? How to achieve 1.8V for UART and GPIOs?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26286i28D2154204864B87/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;-PVDD is used for pad voltage reference and supply of the host interface (HSU, USB, I2C, and SPI) and the GPIOs. so if you use PNEV7462B , you may connect PVDD to an external power, please also note in such kind of case, If PVDD is externally supplied,&amp;nbsp; the Jumper 42 (PVDD_OUT) needs to be set. By setting&amp;nbsp; this Jumper the PVDD_OUT is shorted to GND and the PN7462AU turns off the PVDD&amp;nbsp; LDO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. How to download the firmware on PN7462? Using SWD interface ?&lt;/P&gt;&lt;P&gt;-Yes, exactly.&lt;/P&gt;&lt;P&gt;3. How to properly design the antenna circuit for NFC communication. Is there any antenna chip available on the market or I need to print it on a PCB?&lt;/P&gt;&lt;P&gt;- You may find all you need from the following link: &lt;A class="link-titled" href="http://www.nxp.com/docs/en/application-note/AN11706.pdf" title="http://www.nxp.com/docs/en/application-note/AN11706.pdf"&gt;http://www.nxp.com/docs/en/application-note/AN11706.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and yes, PN7462's HSUART just supports slave mode, so you have to use GPIOs to simulate a UART interface by software. Sorry for the inconvenience that might cause.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jul 2017 09:31:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Need-help-with-PN7462-configuration/m-p/692636#M2468</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2017-07-11T09:31:26Z</dc:date>
    </item>
    <item>
      <title>Re: Need help with PN7462 configuration</title>
      <link>https://community.nxp.com/t5/NFC/Need-help-with-PN7462-configuration/m-p/692637#M2469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;:smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Aug 2018 07:36:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Need-help-with-PN7462-configuration/m-p/692637#M2469</guid>
      <dc:creator>276642088</dc:creator>
      <dc:date>2018-08-10T07:36:15Z</dc:date>
    </item>
  </channel>
</rss>