<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PN7150 NFC Controller Initialization Failed in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN7150-NFC-Controller-Initialization-Failed/m-p/688199#M2422</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to build &amp;nbsp;nfcDemoApp application to run on imx6 based target&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;using PN7150 NFC Controller&lt;/SPAN&gt;. I have followed NXP AN11697 document to build kernel driver and "nfcDemoApp" application as well as install the library. When I run the demo application on the target, it says "NfcService Init Failed Leaving...".&lt;/P&gt;&lt;P&gt;By checking the source code, I know it is due to API function call&amp;nbsp;nativeNfcManager_doInitialize() returning non-zero value. But there is no further detailed explanation of the cause in the "Linux_NFC_API_Guide.html" file.&lt;/P&gt;&lt;P&gt;Can anybody tell me what might be causing non-zero return value of that API function call? How do I know whether the kernel driver or the library were correctly built and installed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;William&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Jun 2017 23:16:21 GMT</pubDate>
    <dc:creator>wjzhang99</dc:creator>
    <dc:date>2017-06-14T23:16:21Z</dc:date>
    <item>
      <title>PN7150 NFC Controller Initialization Failed</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-NFC-Controller-Initialization-Failed/m-p/688199#M2422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to build &amp;nbsp;nfcDemoApp application to run on imx6 based target&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;using PN7150 NFC Controller&lt;/SPAN&gt;. I have followed NXP AN11697 document to build kernel driver and "nfcDemoApp" application as well as install the library. When I run the demo application on the target, it says "NfcService Init Failed Leaving...".&lt;/P&gt;&lt;P&gt;By checking the source code, I know it is due to API function call&amp;nbsp;nativeNfcManager_doInitialize() returning non-zero value. But there is no further detailed explanation of the cause in the "Linux_NFC_API_Guide.html" file.&lt;/P&gt;&lt;P&gt;Can anybody tell me what might be causing non-zero return value of that API function call? How do I know whether the kernel driver or the library were correctly built and installed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;William&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jun 2017 23:16:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-NFC-Controller-Initialization-Failed/m-p/688199#M2422</guid>
      <dc:creator>wjzhang99</dc:creator>
      <dc:date>2017-06-14T23:16:21Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 NFC Controller Initialization Failed</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-NFC-Controller-Initialization-Failed/m-p/688200#M2423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This may useful for you&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-331906"&gt;https://community.nxp.com/docs/DOC-331906&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jun 2017 02:23:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-NFC-Controller-Initialization-Failed/m-p/688200#M2423</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2017-06-21T02:23:50Z</dc:date>
    </item>
  </channel>
</rss>