<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CLRC663-02 and CLRC663-03 INT Pin in NFC</title>
    <link>https://community.nxp.com/t5/NFC/CLRC663-02-and-CLRC663-03-INT-Pin/m-p/686192#M2374</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just wanted to confirm that there is no changes between the two revisions on the functionality of the INT pin?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 May 2017 13:53:11 GMT</pubDate>
    <dc:creator>MikeBrennan</dc:creator>
    <dc:date>2017-05-19T13:53:11Z</dc:date>
    <item>
      <title>CLRC663-02 and CLRC663-03 INT Pin</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-02-and-CLRC663-03-INT-Pin/m-p/686192#M2374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just wanted to confirm that there is no changes between the two revisions on the functionality of the INT pin?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 May 2017 13:53:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-02-and-CLRC663-03-INT-Pin/m-p/686192#M2374</guid>
      <dc:creator>MikeBrennan</dc:creator>
      <dc:date>2017-05-19T13:53:11Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663-02 and CLRC663-03 INT Pin</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-02-and-CLRC663-03-INT-Pin/m-p/686193#M2375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="279806" data-username="MichaelBrennan" href="https://community.nxp.com/people/MichaelBrennan"&gt;Michael&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Their INT (IRQ) functions are same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&amp;nbsp; weidong sun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 May 2017 07:17:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-02-and-CLRC663-03-INT-Pin/m-p/686193#M2375</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2017-05-25T07:17:21Z</dc:date>
    </item>
  </channel>
</rss>