<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NFC Forum type 4A in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NFC-Forum-type-4A/m-p/683822#M2297</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use NFC-explore which has Pn512 nfc Transponder. The NFC Reader library can be used as the Software which has both SPI and I2C Interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The demo explore-nfc Basic uses SPI Interface.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Jul 2017 15:03:11 GMT</pubDate>
    <dc:creator>manojrohitvempa</dc:creator>
    <dc:date>2017-07-04T15:03:11Z</dc:date>
    <item>
      <title>NFC Forum type 4A</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Forum-type-4A/m-p/683820#M2295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please can anyone advise me what devices NXP do which support NFC Forum type 4A with I2C interface.&lt;/P&gt;&lt;P&gt;I have been using the NT3H1101 device but need to use the forum type 4A.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jun 2017 15:45:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Forum-type-4A/m-p/683820#M2295</guid>
      <dc:creator>andrewbarningha</dc:creator>
      <dc:date>2017-06-12T15:45:13Z</dc:date>
    </item>
    <item>
      <title>Re: NFC Forum type 4A</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Forum-type-4A/m-p/683821#M2296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am sorry, but so far we just have NFC Forum type 4A tag without I2C interface.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jun 2017 09:02:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Forum-type-4A/m-p/683821#M2296</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2017-06-21T09:02:44Z</dc:date>
    </item>
    <item>
      <title>Re: NFC Forum type 4A</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Forum-type-4A/m-p/683822#M2297</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use NFC-explore which has Pn512 nfc Transponder. The NFC Reader library can be used as the Software which has both SPI and I2C Interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The demo explore-nfc Basic uses SPI Interface.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jul 2017 15:03:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Forum-type-4A/m-p/683822#M2297</guid>
      <dc:creator>manojrohitvempa</dc:creator>
      <dc:date>2017-07-04T15:03:11Z</dc:date>
    </item>
  </channel>
</rss>