<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: PN7150 - Standby Mode</title>
    <link>https://community.nxp.com/t5/NFC/PN7150-Standby-Mode/m-p/683225#M2275</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you please specify on which platform you measured the voltage, OM5578 or a custom board? please help to clarify.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Jun 2017 08:28:16 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2017-06-02T08:28:16Z</dc:date>
    <item>
      <title>PN7150 - Standby Mode</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Standby-Mode/m-p/683224#M2274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about standby mode in the&amp;nbsp;&amp;nbsp; PN7150 chip. I have a running example &lt;SPAN class="" lang="en"&gt;NXP-NCI LPCXpresso example (SW3241) - NXP-NCI_LPC11xx_example on my uC. I would like very low current consumption on my device so I want to use standby mode. Theoretically, it is enabled. Below a snippet of code and send command and response from PN7150.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;NxpNci_CORE_STANDBY[]={0x2F, 0x00, 0x01, 0x01};&amp;nbsp;&amp;nbsp; &amp;nbsp;/* last byte indicates enable/disable */&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;...&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;NCI &amp;gt;&amp;gt;&amp;nbsp; 0x2f&amp;nbsp; 0x00&amp;nbsp; 0x01&amp;nbsp; 0x01&lt;BR /&gt;NCI &amp;lt;&amp;lt;&amp;nbsp; 0x4f&amp;nbsp; 0x00&amp;nbsp; 0x01&amp;nbsp; 0x00&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;...&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;I measured current on the oscilloscope. These&amp;nbsp; waveforms show voltage drop on 1 Ohm resistor.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20991i3C60BD55B3585F0D/image-size/large?v=v2&amp;amp;px=999" title="scope_1.bmp" alt="scope_1.bmp" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21025iBEA3F4A0340D35E6/image-size/large?v=v2&amp;amp;px=999" title="scope_2.bmp" alt="scope_2.bmp" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;The first graph shows current on listening&amp;nbsp; mode and the second when&amp;nbsp; the&amp;nbsp; card is reading.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;As you can see Imax = 223mA. &lt;SPAN class=""&gt;This is a value that is not consistent with the catalog note. I will add that when I&amp;nbsp; disable standby mode (NCI &amp;gt;&amp;gt;&amp;nbsp; 0x2f&amp;nbsp; 0x00&amp;nbsp; 0x01&amp;nbsp; 0x00). The waveforms looked the same, the current has the same value.&amp;nbsp; Why the current is so large? What could be the reason?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Adrian Pakosinski&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 May 2017 11:35:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Standby-Mode/m-p/683224#M2274</guid>
      <dc:creator>adrianpakosinsk</dc:creator>
      <dc:date>2017-05-17T11:35:18Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 - Standby Mode</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Standby-Mode/m-p/683225#M2275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you please specify on which platform you measured the voltage, OM5578 or a custom board? please help to clarify.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2017 08:28:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Standby-Mode/m-p/683225#M2275</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2017-06-02T08:28:16Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 - Standby Mode</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Standby-Mode/m-p/683226#M2276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kan,&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Thank you for your interest&lt;/SPAN&gt;&lt;/SPAN&gt;. These &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;measurements come from custom board but also I made measurements on OM5578. On OM5578 the charts were similar shape but the voltage was smaller, exactly 120mV when the &amp;nbsp; card is reading.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Thanks,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Adrian&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2017 08:41:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Standby-Mode/m-p/683226#M2276</guid>
      <dc:creator>adrianpakosinsk</dc:creator>
      <dc:date>2017-06-02T08:41:24Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 - Standby Mode</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Standby-Mode/m-p/683227#M2277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think it would be possibly a hardware design issue, please kindly refer to &lt;A class="link-titled" href="http://www.nxp.com/documents/application_note/AN11756.pdf" title="http://www.nxp.com/documents/application_note/AN11756.pdf"&gt;http://www.nxp.com/documents/application_note/AN11756.pdf&lt;/A&gt; for reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2017 09:00:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Standby-Mode/m-p/683227#M2277</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2017-06-02T09:00:50Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 - Standby Mode</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Standby-Mode/m-p/683228#M2278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your answer. I read this document and followed the &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;recommendations&lt;/SPAN&gt;&lt;/SPAN&gt;. &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Is the current 120mA taken by OM5578 is a&amp;nbsp; normal value?&amp;nbsp; (when the card is reading). Maybe on my custom board is some hardware design issue but I think on OM5578 everything should be fine.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Thanks,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Adrian&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2017 09:15:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Standby-Mode/m-p/683228#M2278</guid>
      <dc:creator>adrianpakosinsk</dc:creator>
      <dc:date>2017-06-02T09:15:57Z</dc:date>
    </item>
  </channel>
</rss>