<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: PN7362 UART transmission problem</title>
    <link>https://community.nxp.com/t5/NFC/PN7362-UART-transmission-problem/m-p/682100#M2259</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found the solution, it&amp;nbsp;was an hardware problem. I didn't use the RTS/CTS flow control, so I had to connect the CTS pin to the ground.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Jul 2017 16:02:45 GMT</pubDate>
    <dc:creator>thomasbarreto</dc:creator>
    <dc:date>2017-07-24T16:02:45Z</dc:date>
    <item>
      <title>PN7362 UART transmission problem</title>
      <link>https://community.nxp.com/t5/NFC/PN7362-UART-transmission-problem/m-p/682097#M2256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I work on a projet with the PN7362. I try to use the Host Interface, as an UART.&lt;/P&gt;&lt;P&gt;I configured it and I succeeded to receive frames via the Rx pin, but I&amp;nbsp;fail to transmit until now.&lt;/P&gt;&lt;P&gt;I know the EOT interrupt is never generated because the callback function is never called.&lt;/P&gt;&lt;P&gt;I look the Tx Init register and i find the goud values into.&lt;/P&gt;&lt;P&gt;Could you help me with this problem?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Initialisation :&lt;/P&gt;&lt;P&gt;phhalHif_Config_t s_ConfigNXP_HSUART;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;s_ConfigNXP_HSUART.eInterface = E_HIF_HSU;&amp;nbsp;&lt;BR /&gt; s_ConfigNXP_HSUART.sConfig.sHsuConfig.bIsHsuBoot = 0;&amp;nbsp;&lt;BR /&gt; s_ConfigNXP_HSUART.sConfig.sHsuConfig.bEOF = 8;&amp;nbsp;&lt;BR /&gt; s_ConfigNXP_HSUART.sConfig.sHsuConfig.bStopBits = 1;&amp;nbsp;&lt;BR /&gt; s_ConfigNXP_HSUART.sConfig.sHsuConfig.bDummyBytes = 0;&lt;BR /&gt; s_ConfigNXP_HSUART.eBufferType = E_BUFFER_FORMAT_FREE;&amp;nbsp;&lt;BR /&gt; s_ConfigNXP_HSUART.bShortFrameLen = 0;&amp;nbsp;&lt;BR /&gt; s_ConfigNXP_HSUART.bStoreErrData = 0;&amp;nbsp;&lt;BR /&gt; s_ConfigNXP_HSUART.bHeaderSize = 0;&lt;BR /&gt; s_ConfigNXP_HSUART.bTimeout = 100;&amp;nbsp;&lt;/P&gt;&lt;P&gt;s_ConfigNXP_HSUART.sConfig.sHsuConfig.bBaudRate = E_HSU_BAUDRATE_38_4K;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;phhalHif_Init(&amp;amp;s_ConfigNXP_HSUART, (pphhalHif_Callback_t) &amp;amp;Erreur_Init_UART_Interrupt);&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Transmission :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;phStatus_t e = 0;&lt;BR /&gt; unsigned char ui_TxBuffer[4] = {'C','H','A','R'};&lt;BR /&gt; e = phhalHif_Transmit((uint32_t *)&amp;amp;ui_TxBuffer,sizeof(ui_TxBuffer), (pphhalHif_Callback_t)&amp;amp;ext_SetTxBufferEmptyInterrupt);&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; if (e == 0x0021)printf("INVALID PARAM");&lt;BR /&gt; else if (e== 129)printf("TX ONGOING");&lt;BR /&gt; else if (e== 131)printf("TX LOCKED");&lt;BR /&gt; else if (e== 133)printf("TX PREFETCH");&lt;BR /&gt; else if (e==0x00)printf("SUCCESS");&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Jul 2017 12:09:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7362-UART-transmission-problem/m-p/682097#M2256</guid>
      <dc:creator>thomasbarreto</dc:creator>
      <dc:date>2017-07-03T12:09:30Z</dc:date>
    </item>
    <item>
      <title>Re: PN7362 UART transmission problem</title>
      <link>https://community.nxp.com/t5/NFC/PN7362-UART-transmission-problem/m-p/682098#M2257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="301768" data-username="thomasbarreto" href="https://community.nxp.com/people/thomasbarreto"&gt;thomasbarreto&lt;/A&gt;,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope you are doing great, please check the attached project it uses the HSUART to interact with the PN7462 it should not be much different than the one you are using, just as reference.&lt;/P&gt;&lt;P&gt;- Receive UART data at 9600/8/N1 from Host &lt;BR /&gt;- Execute the next commands depending on received character from UART:&lt;BR /&gt;‘T’ = Run a polling test and return PASS/NO PASS response to host depending if card was detected or not.&lt;BR /&gt;‘O’ = Turn RF field on and leave it on.&lt;BR /&gt;‘F’ = Turn RF field off.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jul 2017 16:30:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7362-UART-transmission-problem/m-p/682098#M2257</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2017-07-11T16:30:43Z</dc:date>
    </item>
    <item>
      <title>Re: PN7362 UART transmission problem</title>
      <link>https://community.nxp.com/t5/NFC/PN7362-UART-transmission-problem/m-p/682099#M2258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;I have the same problem with PN7362 and did not find the solution in the attached example.&lt;/SPAN&gt; &lt;SPAN class=""&gt;You can help me?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sHifConfigs.eBufferType = E_BUFFER_FORMAT_FREE; /* E_BUFFER_FORMAT_FREE */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sHifConfigs.bShortFrameLen = 0 ; // gpkphCfg_EE_HW_HIF-&amp;gt;bShortFrameLen;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sHifConfigs.bStoreErrData = 0 ; // gpkphCfg_EE_HW_HIF-&amp;gt;bStoreErrData;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sHifConfigs.bHeaderSize = 0 ; // gpkphCfg_EE_HW_HIF-&amp;gt;bHeaderSize;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sHifConfigs.bTimeout = 0 ; // gpkphCfg_EE_HW_HIF-&amp;gt;bTimeout;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sHifConfigs.eInterface = E_HIF_HSU;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sHifConfigs.sConfig.sHsuConfig.bIsHsuBoot = 0 ; // gpkphCfg_EE_HW_HIF-&amp;gt;bIsHsuBoot;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sHifConfigs.sConfig.sHsuConfig.bEOF = 8 ; // gpkphCfg_EE_HW_HIF-&amp;gt;bEndOfFrame;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sHifConfigs.sConfig.sHsuConfig.bStopBits = 1 ; //gpkphCfg_EE_HW_HIF-&amp;gt;bStopBits;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sHifConfigs.sConfig.sHsuConfig.bDummyBytes = 3 ; // gpkphCfg_EE_HW_HIF-&amp;gt;bDummyBytes;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sHifConfigs.sConfig.sHsuConfig.bBaudRate = E_HSU_BAUDRATE_9_6K ; //(phhalHif_Hsu_BaudRate_t) gpkphCfg_EE_HW_HIF-&amp;gt;bBaudRate;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;/** Host Interface Initialize */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PH_USER_ASSERT(&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; phhalHif_Init(&amp;amp;sHifConfigs, &amp;amp;phExHif_Hw_Generic_CallBack) == PH_ERR_SUCCESS);&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;Thanks, Giovanni&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jul 2017 15:55:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7362-UART-transmission-problem/m-p/682099#M2258</guid>
      <dc:creator>giovannizani</dc:creator>
      <dc:date>2017-07-18T15:55:17Z</dc:date>
    </item>
    <item>
      <title>Re: PN7362 UART transmission problem</title>
      <link>https://community.nxp.com/t5/NFC/PN7362-UART-transmission-problem/m-p/682100#M2259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found the solution, it&amp;nbsp;was an hardware problem. I didn't use the RTS/CTS flow control, so I had to connect the CTS pin to the ground.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 16:02:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7362-UART-transmission-problem/m-p/682100#M2259</guid>
      <dc:creator>thomasbarreto</dc:creator>
      <dc:date>2017-07-24T16:02:45Z</dc:date>
    </item>
    <item>
      <title>Re: PN7362 UART transmission problem</title>
      <link>https://community.nxp.com/t5/NFC/PN7362-UART-transmission-problem/m-p/682101#M2260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Thomas&lt;/P&gt;&lt;P&gt;thanks for the solution, I &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt; also had to connect the #CTS to the ground&lt;/SPAN&gt;&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Unfortunately I did not find the way to disable flowcontrol via firmware&lt;/SPAN&gt;&lt;/SPAN&gt;, &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;if someone knows the solution would be a good thing for me&lt;/SPAN&gt;&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;Thanks Giovanni&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Sep 2017 12:12:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7362-UART-transmission-problem/m-p/682101#M2260</guid>
      <dc:creator>giovannizani</dc:creator>
      <dc:date>2017-09-05T12:12:56Z</dc:date>
    </item>
  </channel>
</rss>