<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CLRC663 INT Pull Up in NFC</title>
    <link>https://community.nxp.com/t5/NFC/CLRC663-INT-Pull-Up/m-p/679628#M2223</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does the CLRC663 require a pull up resistor on the IRQ output pin or can it drive a uController input without the need of a pull up?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 May 2017 19:33:05 GMT</pubDate>
    <dc:creator>MikeBrennan</dc:creator>
    <dc:date>2017-05-15T19:33:05Z</dc:date>
    <item>
      <title>CLRC663 INT Pull Up</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-INT-Pull-Up/m-p/679628#M2223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does the CLRC663 require a pull up resistor on the IRQ output pin or can it drive a uController input without the need of a pull up?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 May 2017 19:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-INT-Pull-Up/m-p/679628#M2223</guid>
      <dc:creator>MikeBrennan</dc:creator>
      <dc:date>2017-05-15T19:33:05Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 INT Pull Up</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-INT-Pull-Up/m-p/679629#M2224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="279806" data-username="MichaelBrennan" href="https://community.nxp.com/people/MichaelBrennan"&gt;Michael&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; IRQ pin doesn't need to be pulled up!&amp;nbsp; it's driver capability is enough.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&amp;nbsp;&amp;nbsp; Weidong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 May 2017 07:05:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-INT-Pull-Up/m-p/679629#M2224</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2017-05-25T07:05:05Z</dc:date>
    </item>
  </channel>
</rss>