<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Re: Using the CLRC663 ReaderChip with the NFC Library without OS</title>
    <link>https://community.nxp.com/t5/NFC/Using-the-CLRC663-ReaderChip-with-the-NFC-Library-without-OS/m-p/671402#M2110</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to chapter 5 of the following Application Note where you will find the projects which can be configured to run with or without FreeRTOS operating system:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/application-note/AN11211.pdf"&gt;http://www.nxp.com/docs/en/application-note/AN11211.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;To enable/disable FreeRTOS, define your settings in the file “../intfs/ph_NxpBuild_App.h”&lt;/P&gt;&lt;P&gt;E.g. enable FreeRTOS&lt;/P&gt;&lt;P&gt;//#define NXPBUILD__PH_OSAL_NULLOS&lt;/P&gt;&lt;P&gt;#define NXPBUILD__PH_OSAL_FREERTOS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Jul 2017 17:41:53 GMT</pubDate>
    <dc:creator>IvanRuiz</dc:creator>
    <dc:date>2017-07-19T17:41:53Z</dc:date>
    <item>
      <title>Using the CLRC663 ReaderChip with the NFC Library without OS</title>
      <link>https://community.nxp.com/t5/NFC/Using-the-CLRC663-ReaderChip-with-the-NFC-Library-without-OS/m-p/671401#M2109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm searching for an easy way to get the CLRC663 ReaderChip working with the help of the NFC Reader Library without an OS. It Looks like that the Library was designd to have there allways an OS running on the CPU. Is there a possible way to do it without an OS?&lt;/P&gt;&lt;P&gt;Are there some libraries to get the Chip working&amp;nbsp;in an easy way?&lt;/P&gt;&lt;P&gt;Or is it the best way to do the implementation with all the Registers and the command combinations by my self?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jul 2017 09:04:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Using-the-CLRC663-ReaderChip-with-the-NFC-Library-without-OS/m-p/671401#M2109</guid>
      <dc:creator>michaelumundum</dc:creator>
      <dc:date>2017-07-17T09:04:42Z</dc:date>
    </item>
    <item>
      <title>Re: Using the CLRC663 ReaderChip with the NFC Library without OS</title>
      <link>https://community.nxp.com/t5/NFC/Using-the-CLRC663-ReaderChip-with-the-NFC-Library-without-OS/m-p/671402#M2110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to chapter 5 of the following Application Note where you will find the projects which can be configured to run with or without FreeRTOS operating system:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/application-note/AN11211.pdf"&gt;http://www.nxp.com/docs/en/application-note/AN11211.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;To enable/disable FreeRTOS, define your settings in the file “../intfs/ph_NxpBuild_App.h”&lt;/P&gt;&lt;P&gt;E.g. enable FreeRTOS&lt;/P&gt;&lt;P&gt;//#define NXPBUILD__PH_OSAL_NULLOS&lt;/P&gt;&lt;P&gt;#define NXPBUILD__PH_OSAL_FREERTOS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 17:41:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Using-the-CLRC663-ReaderChip-with-the-NFC-Library-without-OS/m-p/671402#M2110</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2017-07-19T17:41:53Z</dc:date>
    </item>
  </channel>
</rss>