<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: MFRC522 NTAG213 range improvements</title>
    <link>https://community.nxp.com/t5/NFC/MFRC522-NTAG213-range-improvements/m-p/653896#M1766</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeremy ST,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In general if the tags have a different antenna size (e.g. the antenna of your NTAG213 is smaller) then different reading distances are expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to improve reading distance then I can suggest 2 options:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1)&lt;/STRONG&gt; Tune the antenna to a lower target impedance, always respecting the MFRC522 maximum output power IDD(TVDD) = 100 mA).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2)&lt;/STRONG&gt; If you have reached the max output power then you can use an RF Amplifier design as described in application note AN1425:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.nxp.com/documents/application_note/AN1425_AN166510.zip?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1" title="http://cache.nxp.com/documents/application_note/AN1425_AN166510.zip?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;http://cache.nxp.com/documents/application_note/AN1425_AN166510.zip&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Feb 2017 01:31:54 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2017-02-13T01:31:54Z</dc:date>
    <item>
      <title>MFRC522 NTAG213 range improvements</title>
      <link>https://community.nxp.com/t5/NFC/MFRC522-NTAG213-range-improvements/m-p/653895#M1765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My company is using MFRC522 to read the ID of Ultralight tags on a custom PCB for a consumer application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However I have found a significant difference in range between different tags. MiFARE Ultralight NTAG213 only have ~2cm of range whilst an older MiFARE Ultralight tag (not certain of the type but suspect NTAG203) has ~5cm of range.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This was confirmed using&amp;nbsp;a 'Arduino compatible' development board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it to be expected for the NTAG213 to have a lower range? How could the range be improved? (we have already tuned the antenna to be resonant and 500ohms)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jeremy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2017 04:50:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MFRC522-NTAG213-range-improvements/m-p/653895#M1765</guid>
      <dc:creator>jeremyst</dc:creator>
      <dc:date>2017-01-30T04:50:07Z</dc:date>
    </item>
    <item>
      <title>Re: MFRC522 NTAG213 range improvements</title>
      <link>https://community.nxp.com/t5/NFC/MFRC522-NTAG213-range-improvements/m-p/653896#M1766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeremy ST,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In general if the tags have a different antenna size (e.g. the antenna of your NTAG213 is smaller) then different reading distances are expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to improve reading distance then I can suggest 2 options:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1)&lt;/STRONG&gt; Tune the antenna to a lower target impedance, always respecting the MFRC522 maximum output power IDD(TVDD) = 100 mA).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2)&lt;/STRONG&gt; If you have reached the max output power then you can use an RF Amplifier design as described in application note AN1425:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.nxp.com/documents/application_note/AN1425_AN166510.zip?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1" title="http://cache.nxp.com/documents/application_note/AN1425_AN166510.zip?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;http://cache.nxp.com/documents/application_note/AN1425_AN166510.zip&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Feb 2017 01:31:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MFRC522-NTAG213-range-improvements/m-p/653896#M1766</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2017-02-13T01:31:54Z</dc:date>
    </item>
  </channel>
</rss>