<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックProblem with Pegoda reader and Mifare Desfire V1 card</title>
    <link>https://community.nxp.com/t5/NFC/Problem-with-Pegoda-reader-and-Mifare-Desfire-V1-card/m-p/491763#M172</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm writing test program for Mifare Desfire V1 card and find the following problem. When I send "Select Application" command to the card via Omnikey 5321 v2 CL SAM reader I have got the following log:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mon May 23 09:42:30 2016&lt;/P&gt;&lt;P&gt;REQUEST:&lt;/P&gt;&lt;P&gt;Command =&amp;nbsp; 0x5A 0x00 0x00 0x00&lt;/P&gt;&lt;P&gt;Request Lenght = 4&lt;/P&gt;&lt;P&gt;Request protocol = CL&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;gt;&amp;gt; 5A 00 00 00&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RESPONSE:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;lt;&amp;lt;Response Lenght = 1&lt;/P&gt;&lt;P&gt;Response status = 0x00000000 - SCARD_S_SUCCESS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;lt;&amp;lt; 00&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;This is a normal answer, all is Ok.&lt;/P&gt;&lt;P&gt;When I send the same command to the RD710 reader I have got the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mon May 23 10:00:12 2016&lt;/P&gt;&lt;P&gt;REQUEST:&lt;/P&gt;&lt;P&gt;Command =&amp;nbsp; 0x5A 0x00 0x00 0x00&lt;/P&gt;&lt;P&gt;Request Lenght = 4&lt;/P&gt;&lt;P&gt;Request protocol = CL&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;gt;&amp;gt; 5A 00 00 00&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RESPONSE:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;lt;&amp;lt;Response Lenght = 6&lt;/P&gt;&lt;P&gt;Response status = 0x00000000 - SCARD_S_SUCCESS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;lt;&amp;lt; 5A 80 25 01 00 00&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anybody explain me for what reason I receive such an answer from the card?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 May 2016 07:12:35 GMT</pubDate>
    <dc:creator>hermannzheboldo</dc:creator>
    <dc:date>2016-05-23T07:12:35Z</dc:date>
    <item>
      <title>Problem with Pegoda reader and Mifare Desfire V1 card</title>
      <link>https://community.nxp.com/t5/NFC/Problem-with-Pegoda-reader-and-Mifare-Desfire-V1-card/m-p/491763#M172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm writing test program for Mifare Desfire V1 card and find the following problem. When I send "Select Application" command to the card via Omnikey 5321 v2 CL SAM reader I have got the following log:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mon May 23 09:42:30 2016&lt;/P&gt;&lt;P&gt;REQUEST:&lt;/P&gt;&lt;P&gt;Command =&amp;nbsp; 0x5A 0x00 0x00 0x00&lt;/P&gt;&lt;P&gt;Request Lenght = 4&lt;/P&gt;&lt;P&gt;Request protocol = CL&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;gt;&amp;gt; 5A 00 00 00&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RESPONSE:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;lt;&amp;lt;Response Lenght = 1&lt;/P&gt;&lt;P&gt;Response status = 0x00000000 - SCARD_S_SUCCESS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;lt;&amp;lt; 00&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;This is a normal answer, all is Ok.&lt;/P&gt;&lt;P&gt;When I send the same command to the RD710 reader I have got the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mon May 23 10:00:12 2016&lt;/P&gt;&lt;P&gt;REQUEST:&lt;/P&gt;&lt;P&gt;Command =&amp;nbsp; 0x5A 0x00 0x00 0x00&lt;/P&gt;&lt;P&gt;Request Lenght = 4&lt;/P&gt;&lt;P&gt;Request protocol = CL&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;gt;&amp;gt; 5A 00 00 00&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RESPONSE:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;lt;&amp;lt;Response Lenght = 6&lt;/P&gt;&lt;P&gt;Response status = 0x00000000 - SCARD_S_SUCCESS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;lt;&amp;lt; 5A 80 25 01 00 00&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anybody explain me for what reason I receive such an answer from the card?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 May 2016 07:12:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Problem-with-Pegoda-reader-and-Mifare-Desfire-V1-card/m-p/491763#M172</guid>
      <dc:creator>hermannzheboldo</dc:creator>
      <dc:date>2016-05-23T07:12:35Z</dc:date>
    </item>
  </channel>
</rss>