<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: NFC Cockpit issue under Windows 10</title>
    <link>https://community.nxp.com/t5/NFC/NFC-Cockpit-issue-under-Windows-10/m-p/650817#M1711</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After a new positive test done under Windows XP running in a VM on the same computer, the issue met under W10 is clearly related to the installation of the PN7462 VCOM driver.&lt;/P&gt;&lt;P&gt;To be continued...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Oct 2016 12:57:01 GMT</pubDate>
    <dc:creator>jean-pierrefort</dc:creator>
    <dc:date>2016-10-19T12:57:01Z</dc:date>
    <item>
      <title>NFC Cockpit issue under Windows 10</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Cockpit-issue-under-Windows-10/m-p/650816#M1710</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'am trying to work with the PNEV7462B eval board and the NFC Cockpit tool (v1.3.0.0) under Windows 10.&lt;/P&gt;&lt;P&gt;I have successfully updated the board (firmware and eeprom) through the mass storage 'channel'.&lt;/P&gt;&lt;P&gt;After reboot, a new USB virtual serial port appeared (COM11) but Cockpit doesn't see it. The port selector combo is empty.&lt;/P&gt;&lt;P&gt;I also reinstalled the VCOM driver (forcing Windows 10 to install unsigned drivers) but the result is the same.&lt;/P&gt;&lt;P&gt;Is there a known issue around this?&lt;/P&gt;&lt;P&gt;Thanks in advance for your help.&lt;/P&gt;&lt;P&gt;--&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jean-Pierre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Oct 2016 08:55:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Cockpit-issue-under-Windows-10/m-p/650816#M1710</guid>
      <dc:creator>jean-pierrefort</dc:creator>
      <dc:date>2016-10-19T08:55:07Z</dc:date>
    </item>
    <item>
      <title>Re: NFC Cockpit issue under Windows 10</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Cockpit-issue-under-Windows-10/m-p/650817#M1711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After a new positive test done under Windows XP running in a VM on the same computer, the issue met under W10 is clearly related to the installation of the PN7462 VCOM driver.&lt;/P&gt;&lt;P&gt;To be continued...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Oct 2016 12:57:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Cockpit-issue-under-Windows-10/m-p/650817#M1711</guid>
      <dc:creator>jean-pierrefort</dc:creator>
      <dc:date>2016-10-19T12:57:01Z</dc:date>
    </item>
    <item>
      <title>Re: NFC Cockpit issue under Windows 10</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Cockpit-issue-under-Windows-10/m-p/650818#M1712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Finally it works after reinstalling the VCOM driver using another method:&lt;/P&gt;&lt;P&gt;peripherals-&amp;gt;update driver-&amp;gt;choose driver in list-&amp;gt;select PN7462AU VCOM Port.&lt;/P&gt;&lt;P&gt;The device name now appears as&amp;nbsp;PN7462AU VCOM (COM11)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Oct 2016 14:15:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Cockpit-issue-under-Windows-10/m-p/650818#M1712</guid>
      <dc:creator>jean-pierrefort</dc:creator>
      <dc:date>2016-10-19T14:15:20Z</dc:date>
    </item>
  </channel>
</rss>