<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Procedure to enable AFI password in ICODE SLIX tag in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Procedure-to-enable-AFI-password-in-ICODE-SLIX-tag/m-p/649528#M1689</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Morten Moller,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The attached script is for RC663 red board supporting ICODE SLIX tags, please kindly refer to it for details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Apr 2017 07:04:24 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2017-04-26T07:04:24Z</dc:date>
    <item>
      <title>Procedure to enable AFI password in ICODE SLIX tag</title>
      <link>https://community.nxp.com/t5/NFC/Procedure-to-enable-AFI-password-in-ICODE-SLIX-tag/m-p/649527#M1688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I might be asking this question in the wrong forum, so feel free to move this to the proper location.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am developing an application that needs to enable and use the AFI-password protection feature in ICODE SLIX tags. While the command reference states which ISO 15693 commands to use, it does not state in which order.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know which ISO 15693 commands and the sequence of them is needed in order to enable AFI-password protection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am aware of the procedure to "set" password (get random number -&amp;gt; XOR -&amp;gt; set password), but I need to be able to activate it in the tags in the first place.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So far what I have read is that I must use the ISO 15693 0xA6 command (password protect EAS/AFI), but that requires the password to be set. In order for me to do this there must be a default password on which I need to do the above operation. But what is the default password? is it just plain 0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope someone is able to help with this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-M.G.Moller&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Apr 2017 12:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Procedure-to-enable-AFI-password-in-ICODE-SLIX-tag/m-p/649527#M1688</guid>
      <dc:creator>mortenmoller</dc:creator>
      <dc:date>2017-04-04T12:44:39Z</dc:date>
    </item>
    <item>
      <title>Re: Procedure to enable AFI password in ICODE SLIX tag</title>
      <link>https://community.nxp.com/t5/NFC/Procedure-to-enable-AFI-password-in-ICODE-SLIX-tag/m-p/649528#M1689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Morten Moller,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The attached script is for RC663 red board supporting ICODE SLIX tags, please kindly refer to it for details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2017 07:04:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Procedure-to-enable-AFI-password-in-ICODE-SLIX-tag/m-p/649528#M1689</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2017-04-26T07:04:24Z</dc:date>
    </item>
  </channel>
</rss>