<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PN532 ISO14443-4 communication Issue in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN532-ISO14443-4-communication-Issue/m-p/641284#M1515</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mr Kan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for this very very long delay.&amp;nbsp; I was busy on a new project and now, I come back to this issue.&amp;nbsp; It's really not fixed.&amp;nbsp; I would like to transfer data as fast as possible but I noticed that the PN532 device sends very slow the data.&amp;nbsp; What information do you need to understand more the problem?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the PN512 to receive the data and I noticed that it takes more than 10 ms to receive the first 64 bytes packet.&amp;nbsp; It's too slow when I initialized the speed to 424 kbps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Feb 2017 18:08:15 GMT</pubDate>
    <dc:creator>christian_greni</dc:creator>
    <dc:date>2017-02-23T18:08:15Z</dc:date>
    <item>
      <title>PN532 ISO14443-4 communication Issue</title>
      <link>https://community.nxp.com/t5/NFC/PN532-ISO14443-4-communication-Issue/m-p/641281#M1512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to communicate very fast from a PN532 (PICC) device with a PN512 (PCD) Initiator using the ISO14443-4. &amp;nbsp;I have a lot of data to transfer from PICC to PCD. &amp;nbsp;Since the PN512 has only 64 bytes in the FIFO, the PN532 uses the chaining mode to transfer 256 bytes. &amp;nbsp;I use the command 0x8E in PN532 to send 256 bytes and I can see that there're 4 x 64-bytes transmitted from PN532 to PN512. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attached an image to show the first 64 bytes transmission.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to understand why it takes several ms for the PN532 to transmit the first 64 bytes. &amp;nbsp;Is there a way to improve that? &amp;nbsp;To reduce the process time to send the first packet?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please, refer to the image to understand my issue. &amp;nbsp;I took several days before posting this message. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Dec 2016 14:41:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN532-ISO14443-4-communication-Issue/m-p/641281#M1512</guid>
      <dc:creator>christiangrenie</dc:creator>
      <dc:date>2016-12-01T14:41:38Z</dc:date>
    </item>
    <item>
      <title>Re: PN532 ISO14443-4 communication Issue</title>
      <link>https://community.nxp.com/t5/NFC/PN532-ISO14443-4-communication-Issue/m-p/641282#M1513</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did a small mistake in the picture. &amp;nbsp;It takes 9.9 ms to receive (PCD) the first packet. &amp;nbsp;At 424 kbits per seconds, a 64 bytes should take around ~1.5 ms, but why does the PN532 take 9 ms to send the first packet and also the next ones. &amp;nbsp;The PN532 firmware version is 1.6. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attach a new picture... &amp;nbsp;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11164iCE821C118CCCE198/image-size/large?v=v2&amp;amp;px=999" title="424 kbits issue.png" alt="424 kbits issue.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Dec 2016 13:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN532-ISO14443-4-communication-Issue/m-p/641282#M1513</guid>
      <dc:creator>christiangrenie</dc:creator>
      <dc:date>2016-12-02T13:22:42Z</dc:date>
    </item>
    <item>
      <title>Re: PN532 ISO14443-4 communication Issue</title>
      <link>https://community.nxp.com/t5/NFC/PN532-ISO14443-4-communication-Issue/m-p/641283#M1514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Christian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you please provide more details on the setup regarding PN532 and PN512? Thanks for your patience!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 06:39:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN532-ISO14443-4-communication-Issue/m-p/641283#M1514</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2016-12-09T06:39:34Z</dc:date>
    </item>
    <item>
      <title>Re: PN532 ISO14443-4 communication Issue</title>
      <link>https://community.nxp.com/t5/NFC/PN532-ISO14443-4-communication-Issue/m-p/641284#M1515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mr Kan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for this very very long delay.&amp;nbsp; I was busy on a new project and now, I come back to this issue.&amp;nbsp; It's really not fixed.&amp;nbsp; I would like to transfer data as fast as possible but I noticed that the PN532 device sends very slow the data.&amp;nbsp; What information do you need to understand more the problem?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the PN512 to receive the data and I noticed that it takes more than 10 ms to receive the first 64 bytes packet.&amp;nbsp; It's too slow when I initialized the speed to 424 kbps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Feb 2017 18:08:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN532-ISO14443-4-communication-Issue/m-p/641284#M1515</guid>
      <dc:creator>christian_greni</dc:creator>
      <dc:date>2017-02-23T18:08:15Z</dc:date>
    </item>
  </channel>
</rss>