<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックNFC NTAG I2C</title>
    <link>https://community.nxp.com/t5/NFC/NFC-NTAG-I2C/m-p/638230#M1452</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi....We have NXP-NTAG I2C device (OM5569/NT312A), which we are exploring to port it on Linux Ubuntu PC. When we connect the device to Linux (UBUNTU) PC via USB, we have an interface /dev/usb/hiddev0 been created, but while we are trying to read/write from/into the device (hiddev0), the calls are getting failed. Even write IOCTL calls are also getting failed. Our requirement is to send/receive a file to/from the device EEPROM and able to read that file from the reader. So can I request you to get some NDEF sample code written for Linux on USB interface to read/write from/into the device EEPROM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Sep 2016 06:13:54 GMT</pubDate>
    <dc:creator>shankary</dc:creator>
    <dc:date>2016-09-21T06:13:54Z</dc:date>
    <item>
      <title>NFC NTAG I2C</title>
      <link>https://community.nxp.com/t5/NFC/NFC-NTAG-I2C/m-p/638230#M1452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi....We have NXP-NTAG I2C device (OM5569/NT312A), which we are exploring to port it on Linux Ubuntu PC. When we connect the device to Linux (UBUNTU) PC via USB, we have an interface /dev/usb/hiddev0 been created, but while we are trying to read/write from/into the device (hiddev0), the calls are getting failed. Even write IOCTL calls are also getting failed. Our requirement is to send/receive a file to/from the device EEPROM and able to read that file from the reader. So can I request you to get some NDEF sample code written for Linux on USB interface to read/write from/into the device EEPROM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 06:13:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-NTAG-I2C/m-p/638230#M1452</guid>
      <dc:creator>shankary</dc:creator>
      <dc:date>2016-09-21T06:13:54Z</dc:date>
    </item>
  </channel>
</rss>