<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックQuestion Regarding RFIDDiscover Setup for MIFARE SAM AV3 Evaluation Board</title>
    <link>https://community.nxp.com/t5/NFC/Question-Regarding-RFIDDiscover-Setup-for-MIFARE-SAM-AV3/m-p/2395309#M14358</link>
    <description>&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Hello,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;I am using the MIFARE SAM AV3 Evaluation Board (UM11316). According to Section 7.4.1, RFIDDiscover requires the board to be connected through the ISO7816 interface using an Ashling IN-CLA7816 adapter and a compatible PC/SC reader.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Could you please clarify:&lt;/FONT&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Is the Ashling IN-CLA7816 adapter mandatory, or can another ISO7816 adapter be used?&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Which PC/SC readers have been validated or are officially supported with the evaluation board and RFIDDiscover?&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Can you recommend a reader that is currently available for purchase?&lt;/FONT&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Thank you.&lt;/FONT&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 15 Jul 2026 09:28:39 GMT</pubDate>
    <dc:creator>boussihak</dc:creator>
    <dc:date>2026-07-15T09:28:39Z</dc:date>
    <item>
      <title>Question Regarding RFIDDiscover Setup for MIFARE SAM AV3 Evaluation Board</title>
      <link>https://community.nxp.com/t5/NFC/Question-Regarding-RFIDDiscover-Setup-for-MIFARE-SAM-AV3/m-p/2395309#M14358</link>
      <description>&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Hello,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;I am using the MIFARE SAM AV3 Evaluation Board (UM11316). According to Section 7.4.1, RFIDDiscover requires the board to be connected through the ISO7816 interface using an Ashling IN-CLA7816 adapter and a compatible PC/SC reader.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Could you please clarify:&lt;/FONT&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Is the Ashling IN-CLA7816 adapter mandatory, or can another ISO7816 adapter be used?&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Which PC/SC readers have been validated or are officially supported with the evaluation board and RFIDDiscover?&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Can you recommend a reader that is currently available for purchase?&lt;/FONT&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Thank you.&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jul 2026 09:28:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Question-Regarding-RFIDDiscover-Setup-for-MIFARE-SAM-AV3/m-p/2395309#M14358</guid>
      <dc:creator>boussihak</dc:creator>
      <dc:date>2026-07-15T09:28:39Z</dc:date>
    </item>
    <item>
      <title>Re: Question Regarding RFIDDiscover Setup for MIFARE SAM AV3 Evaluation Board</title>
      <link>https://community.nxp.com/t5/NFC/Question-Regarding-RFIDDiscover-Setup-for-MIFARE-SAM-AV3/m-p/2395563#M14359</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262979"&gt;@boussihak&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/MIFSAMAV3-DEV-KIT" target="_blank"&gt;MIFARE SAM AV3 Development Kit&lt;/A&gt; should already include a ISO/IEC 7816 Smart Card Reader Adapter that you can use.&lt;/P&gt;
&lt;P&gt;Also, I will recommend you using &lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/CLRD730" target="_blank"&gt;PEGODA Contactless Smart Card Reader&lt;/A&gt;; this device can be used in PC/SC mode and integrates a contact card slot.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jul 2026 18:07:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Question-Regarding-RFIDDiscover-Setup-for-MIFARE-SAM-AV3/m-p/2395563#M14359</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2026-07-15T18:07:50Z</dc:date>
    </item>
  </channel>
</rss>